Data structure of the query_block_status_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::elem_index
The client model element index.
Definition at line
10628
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_complete#
uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::block_complete
Non-zero if the block is complete.
Definition at line
10629
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_complete#
uint8_t sl_btmesh_evt_mbt_client_query_block_status_complete_s::transfer_complete
Non-zero if the transfer is complete.
Definition at line
10630
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h