Data structure of the start_block_complete event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_mbt_client_start_block_complete_s::elem_index
The client model element index.
Definition at line
10502
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_number#
uint16_t sl_btmesh_evt_mbt_client_start_block_complete_s::block_number
The index number of the block.
Definition at line
10503
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
block_size#
uint32_t sl_btmesh_evt_mbt_client_start_block_complete_s::block_size
The size of the block.
Definition at line
10504
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h