List of Command Classes supported when device is not included, included insecurely or included securely.

Public Attributes#

List of UNsecure supported command classes.

List of UNsecure supported command classes in secure network.

List of Secure supported command classes.

Public Attribute Documentation#

UnSecureIncludedCC#

SCommandClassList_t SCommandClassSet_t::UnSecureIncludedCC

List of UNsecure supported command classes.

Available when node is NOT included or UNsecure included


Definition at line 1320 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SecureIncludedUnSecureCC#

SCommandClassList_t SCommandClassSet_t::SecureIncludedUnSecureCC

List of UNsecure supported command classes in secure network.

Available when node is secure included


Definition at line 1321 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SecureIncludedSecureCC#

SCommandClassList_t SCommandClassSet_t::SecureIncludedSecureCC

List of Secure supported command classes.

Available when node is secure included


Definition at line 1322 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h