Public Attributes#

void(*

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.

uint8_t

Public Attribute Documentation#

Handle#

void(* SSendSlaveNodeInformation::Handle) (void)

Definition at line 1446 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

sourceId#

node_id_t SSendSlaveNodeInformation::sourceId

Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.


Definition at line 1449 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

destinationId#

node_id_t SSendSlaveNodeInformation::destinationId

Definition at line 1450 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

txOptions#

uint8_t SSendSlaveNodeInformation::txOptions

Definition at line 1451 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h