Public Attribute Documentation#

FrameConfig#

STransmitFrameConfig SSendDataEx::FrameConfig

Definition at line 1694 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DestNodeId#

node_id_t SSendDataEx::DestNodeId

Definition at line 1695 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SourceNodeId#

node_id_t SSendDataEx::SourceNodeId

Definition at line 1696 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TransmitSecurityOptions#

uint8_t SSendDataEx::TransmitSecurityOptions

Definition at line 1697 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TransmitOptions2#

uint8_t SSendDataEx::TransmitOptions2

Definition at line 1698 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

eKeyType#

enum SECURITY_KEY SSendDataEx::eKeyType

Definition at line 1699 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h