Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

Major#

uint8_t SProtocolVersion::Major

Definition at line 1530 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

Minor#

uint8_t SProtocolVersion::Minor

Definition at line 1531 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

Revision#

uint8_t SProtocolVersion::Revision

Definition at line 1532 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h