Public Attribute Documentation#

NodeMask#

NODE_MASK_TYPE SReceiveMulti::NodeMask

Definition at line 2164 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

Payload#

UReceiveCmdPayload SReceiveMulti::Payload

Definition at line 2165 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

iCommandLength#

uint8_t SReceiveMulti::iCommandLength

Definition at line 2166 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

RxOptions#

RECEIVE_OPTIONS_TYPE SReceiveMulti::RxOptions

Definition at line 2167 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h