Public Attributes#

True if this node is always on air.

Public Attribute Documentation#

NodeId#

node_id_t SVirtualSlaveNodeInfo_t::NodeId

Definition at line 1620 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

bListening#

bool SVirtualSlaveNodeInfo_t::bListening

Definition at line 1621 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

NodeType#

APPL_NODE_TYPE SVirtualSlaveNodeInfo_t::NodeType

True if this node is always on air.


Definition at line 1622 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

CommandClasses#

SCommandClassList_t SVirtualSlaveNodeInfo_t::CommandClasses

Definition at line 1623 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h