Transmit Parameters Union used by SZwaveTransmitPackage.
Public Attributes#
Public Attribute Documentation#
ExploreInclusionRequest#
SExploreInclusionRequest UTransmitParameters::ExploreInclusionRequest
Definition at line
2007
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
ExploreExclusionRequest#
SExploreExclusionRequest UTransmitParameters::ExploreExclusionRequest
Definition at line
2008
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
NetworkUpdateRequest#
SNetworkUpdateRequest UTransmitParameters::NetworkUpdateRequest
Definition at line
2009
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
NodeInfoRequest#
SNodeInfoRequest UTransmitParameters::NodeInfoRequest
Definition at line
2010
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
NodeInfo#
SNodeInfo UTransmitParameters::NodeInfo
Definition at line
2011
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
IncludedNodeInfo#
SIncludedNodeInfo UTransmitParameters::IncludedNodeInfo
Definition at line
2012
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
Test#
STest UTransmitParameters::Test
Definition at line
2013
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendData#
SSendData UTransmitParameters::SendData
Definition at line
2015
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendDataEx#
SSendDataEx UTransmitParameters::SendDataEx
Definition at line
2016
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendDataBridge#
SSendDataBridge UTransmitParameters::SendDataBridge
Definition at line
2017
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendDataMulti#
SSendDataMulti UTransmitParameters::SendDataMulti
Definition at line
2018
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendDataMultiEx#
SSendDataMultiEx UTransmitParameters::SendDataMultiEx
Definition at line
2019
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendDataMultiBridge#
SSendDataMultiBridge UTransmitParameters::SendDataMultiBridge
Definition at line
2020
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SetSucNodeId#
SSetSucNodeId UTransmitParameters::SetSucNodeId
Definition at line
2022
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendSucNodeId#
SSendSucNodeId UTransmitParameters::SendSucNodeId
Definition at line
2023
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
AssignReturnRoute#
SAssignReturnRoute UTransmitParameters::AssignReturnRoute
Definition at line
2024
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
DeleteReturnRoute#
SDeleteReturnRoute UTransmitParameters::DeleteReturnRoute
Definition at line
2025
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendReplication#
SSendReplication UTransmitParameters::SendReplication
Definition at line
2026
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendReplicationReceiveComplete#
SSendReplicationReceiveComplete UTransmitParameters::SendReplicationReceiveComplete
Definition at line
2027
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
SendSlaveNodeInformation#
SSendSlaveNodeInformation UTransmitParameters::SendSlaveNodeInformation
Definition at line
2028
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h
RequestNewRouteDestinations#
SRequestNewRouteDestinations UTransmitParameters::RequestNewRouteDestinations
Definition at line
2030
of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h