Network Info.

Public Attribute Documentation#

eInclusionState#

EInclusionState_t SNetworkInfo::eInclusionState

Definition at line 1547 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SucNodeId#

node_id_t SNetworkInfo::SucNodeId

Definition at line 1548 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

SecurityKeys#

uint8_t SNetworkInfo::SecurityKeys

Definition at line 1549 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

NodeId#

node_id_t SNetworkInfo::NodeId

Definition at line 1550 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

HomeId#

uint32_t SNetworkInfo::HomeId

Definition at line 1551 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

MaxPayloadSize#

uint16_t SNetworkInfo::MaxPayloadSize

Definition at line 1552 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h