Public Attributes#

void(*

Public Attribute Documentation#

Handle#

void(* SNodeInfo::Handle) (void)

Definition at line 1298 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

DestNodeId#

node_id_t SNodeInfo::DestNodeId

Definition at line 1301 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h

TransmitOptions#

uint8_t SNodeInfo::TransmitOptions

Definition at line 1302 of file /mnt/raid/workspaces/ws.WDdsgIAV6/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_application_transport_interface.h