USB_StringDescriptor_TypeDef Struct Reference
USB String Descriptor.
#include <em_usb.h>
Data Fields | |
uint8_t | len |
Size of this descriptor in bytes. | |
uint8_t | type |
Constant STRING Descriptor Type. | |
char16_t | name [] |
The string encoded with UTF-16LE UNICODE charset. | |
USB String Descriptor.
Field Documentation
◆ len
uint8_t USB_StringDescriptor_TypeDef::len |
Size of this descriptor in bytes.
◆ type
uint8_t USB_StringDescriptor_TypeDef::type |
Constant STRING Descriptor Type.
◆ name
char16_t USB_StringDescriptor_TypeDef::name[] |
The string encoded with UTF-16LE UNICODE charset.