Entropy
Description
Random number generators.
API for getting randomness from the Secure Element True Random Number Generator (TRNG).
Functions | |
sl_status_t | sl_se_get_random (sl_se_command_context_t *cmd_ctx, void *data, uint32_t num_bytes) |
Get random data from hardware TRNG. | |
Function Documentation
◆ sl_se_get_random()
sl_status_t sl_se_get_random | ( | sl_se_command_context_t * | cmd_ctx, |
void * | data, |
||
uint32_t | num_bytes |
||
) |
Get random data from hardware TRNG.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [out] data
Random data from TRNG. [in] num_bytes
Length of data request.
- Returns
- Status code, sl_status.h.