Cipher
Description
Symmetric encryption, AEAD and MAC.
API for performing symmetric encryption, Authenticated Encryption and Additional Data (AEAD) operations, and computing Message Authentication Codes (MACs) using the Secure Element.
Data Structures | |
struct | sl_se_cmac_streaming_context_t |
CMAC streaming context. | |
struct | sl_se_gcm_streaming_context_t |
GCM streaming context. | |
Functions | |
sl_status_t | sl_se_aes_crypt_ecb (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, size_t length, const unsigned char *input, unsigned char *output) |
AES-ECB block encryption/decryption. | |
sl_status_t | sl_se_aes_crypt_cbc (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, size_t length, unsigned char iv[16], const unsigned char *input, unsigned char *output) |
AES-CBC buffer encryption/decryption. | |
sl_status_t | sl_se_aes_crypt_cfb128 (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, size_t length, uint32_t *iv_off, unsigned char iv[16], const unsigned char *input, unsigned char *output) |
AES-CFB128 buffer encryption/decryption. | |
sl_status_t | sl_se_aes_crypt_cfb8 (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, size_t length, unsigned char iv[16], const unsigned char *input, unsigned char *output) |
AES-CFB8 buffer encryption/decryption. | |
sl_status_t | sl_se_aes_crypt_ctr (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, uint32_t *nc_off, unsigned char nonce_counter[16], unsigned char stream_block[16], const unsigned char *input, unsigned char *output) |
AES-CTR buffer encryption/decryption. | |
sl_status_t | sl_se_ccm_encrypt_and_tag (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char *iv, size_t iv_len, const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, unsigned char *tag, size_t tag_len) |
AES-CCM buffer encryption. | |
sl_status_t | sl_se_ccm_auth_decrypt (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char *iv, size_t iv_len, const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, const unsigned char *tag, size_t tag_len) |
AES-CCM buffer decryption. | |
sl_status_t | sl_se_gcm_crypt_and_tag (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, size_t length, const unsigned char *iv, size_t iv_len, const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, size_t tag_len, unsigned char *tag) |
This function performs GCM encryption or decryption of a buffer. | |
sl_status_t | sl_se_gcm_auth_decrypt (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char *iv, size_t iv_len, const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, size_t tag_len, const unsigned char *tag) |
This function performs a GCM authenticated decryption of a buffer. | |
sl_status_t | sl_se_cmac (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, const unsigned char *input, size_t input_len, unsigned char *output) |
This function calculates the full generic CMAC on the input buffer with the provided key. | |
sl_status_t | sl_se_cmac_starts (sl_se_cmac_streaming_context_t *cmac_ctx, sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key) |
Prepare a CMAC streaming command context object. | |
sl_status_t | sl_se_cmac_update (sl_se_cmac_streaming_context_t *cmac_ctx, const uint8_t *input, size_t input_len) |
This function feeds an input buffer into an ongoing CMAC computation. | |
sl_status_t | sl_se_cmac_finish (sl_se_cmac_streaming_context_t *cmac_ctx, uint8_t *output) |
Finish a CMAC streaming operation and return the resulting CMAC tag. | |
sl_status_t | sl_se_gcm_starts (sl_se_gcm_streaming_context_t *gcm_ctx, sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_cipher_operation_t mode, const uint8_t *iv, size_t iv_len, const uint8_t *add, size_t add_len) |
Prepare a GCM streaming command context object. | |
sl_status_t | sl_se_gcm_update (sl_se_gcm_streaming_context_t *gcm_ctx, size_t length, const uint8_t *input, uint8_t *output) |
This function feeds an input buffer into an ongoing GCM computation. | |
sl_status_t | sl_se_gcm_finish (sl_se_gcm_streaming_context_t *gcm_ctx, uint8_t *tag, size_t tag_len) |
Finish a GCM streaming operation and return the resulting GCM tag. | |
sl_status_t | sl_se_hmac (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, sl_se_hash_type_t hash_type, const uint8_t *message, size_t message_len, uint8_t *output, size_t output_len) |
Compute a HMAC on a full message. | |
sl_status_t | sl_se_chacha20_crypt (sl_se_command_context_t *cmd_ctx, sl_se_cipher_operation_t mode, const sl_se_key_descriptor_t *key, size_t length, const unsigned char initial_counter[4], const unsigned char nonce[12], const unsigned char *input, unsigned char *output) |
ChaCha20 buffer encryption/decryption, as defined by RFC8439 section 2.4. | |
sl_status_t | sl_se_chacha20_poly1305_encrypt_and_tag (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char nonce[12], const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, unsigned char *tag) |
ChaCha20-Poly1305 authenticated encryption with additional data, as defined by RFC8439 section 2.8. | |
sl_status_t | sl_se_chacha20_poly1305_auth_decrypt (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char nonce[12], const unsigned char *add, size_t add_len, const unsigned char *input, unsigned char *output, const unsigned char tag[16]) |
ChaCha20-Poly1305 authenticated decryption with additional data, as defined by RFC8439 section 2.8. | |
sl_status_t | sl_se_poly1305_genkey_tag (sl_se_command_context_t *cmd_ctx, const sl_se_key_descriptor_t *key, size_t length, const unsigned char nonce[12], const unsigned char *input, unsigned char *tag) |
Generate a Poly1305 MAC (message authentication code) for a given message using an ephemeral key derived using ChaCha20. | |
Macros | |
#define | SL_SE_CMAC_STREAMING_INIT_DEFAULT { NULL, { 0 }, { 0 }, 0 } |
Initial values for CMAC streaming context struct sl_se_cmac_streaming_context_t. | |
#define | SL_SE_GCM_STREAMING_INIT_DEFAULT |
Initial values for AES-GCM streaming context struct sl_se_gcm_streaming_context_t. | |
Enumerations | |
enum | sl_se_cipher_operation_t { SL_SE_ENCRYPT, SL_SE_DECRYPT } |
Cipher operation types. | |
Function Documentation
◆ sl_se_aes_crypt_ecb()
sl_status_t sl_se_aes_crypt_ecb | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
size_t | length, |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
AES-ECB block encryption/decryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] mode
Crypto operation type (encryption or decryption). [in] length
Length of the input data. [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_aes_crypt_cbc()
sl_status_t sl_se_aes_crypt_cbc | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
size_t | length, |
||
unsigned char | iv[16], |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
AES-CBC buffer encryption/decryption.
- Note
- Length should be a multiple of the block size (16 bytes).
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] mode
Crypto operation type (encryption or decryption). [in] length
Length of the input data. [in,out] iv
Initialization vector (updated after use). [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_aes_crypt_cfb128()
sl_status_t sl_se_aes_crypt_cfb128 | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
size_t | length, |
||
uint32_t * | iv_off, |
||
unsigned char | iv[16], |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
AES-CFB128 buffer encryption/decryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] mode
Crypto operation type (encryption or decryption). [in] length
Length of the input data. [in,out] iv_off
Offset in IV (updated after use). [in,out] iv
Initialization vector (updated after use). [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_aes_crypt_cfb8()
sl_status_t sl_se_aes_crypt_cfb8 | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
size_t | length, |
||
unsigned char | iv[16], |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
AES-CFB8 buffer encryption/decryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] mode
Crypto operation type (encryption or decryption). [in] length
Length of the input data. [in,out] iv
Initialization vector (updated after use). [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_aes_crypt_ctr()
sl_status_t sl_se_aes_crypt_ctr | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
uint32_t * | nc_off, |
||
unsigned char | nonce_counter[16], |
||
unsigned char | stream_block[16], |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
AES-CTR buffer encryption/decryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
Length of the input data. [in] nc_off
The offset in the current stream_block (for resuming within current cipher stream). The offset pointer to should be 0 at the start of a stream. [in,out] nonce_counter
The 128-bit nonce and counter. [in,out] stream_block
The saved stream-block for resuming (updated after use). [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_ccm_encrypt_and_tag()
sl_status_t sl_se_ccm_encrypt_and_tag | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char * | iv, |
||
size_t | iv_len, |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
unsigned char * | tag, |
||
size_t | tag_len |
||
) |
AES-CCM buffer encryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
The length of the input data in Bytes. [in] iv
Initialization vector (nonce). [in] iv_len
The length of the IV in Bytes: 7, 8, 9, 10, 11, 12, or 13. [in] add
The additional data field. [in] add_len
The length of additional data in Bytes. [in] input
The buffer holding the input data. [out] output
The buffer holding the output data. Must be at least length
Bytes wide.[in,out] tag
The buffer holding the tag. [in] tag_len
The length of the tag to generate in Bytes: 4, 6, 8, 10, 12, 14 or 16.
- Returns
- Status code, sl_status.h.
◆ sl_se_ccm_auth_decrypt()
sl_status_t sl_se_ccm_auth_decrypt | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char * | iv, |
||
size_t | iv_len, |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
const unsigned char * | tag, |
||
size_t | tag_len |
||
) |
AES-CCM buffer decryption.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
The length of the input data in Bytes. [in] iv
Initialization vector. [in] iv_len
The length of the IV in Bytes: 7, 8, 9, 10, 11, 12, or 13. [in] add
The additional data field. [in] add_len
The length of additional data in Bytes. [in] input
The buffer holding the input data. [out] output
The buffer holding the output data. Must be at least length
Bytes wide.[in] tag
The buffer holding the tag. [in] tag_len
The length of the tag in Bytes.
- Returns
- Status code, sl_status.h.
◆ sl_se_gcm_crypt_and_tag()
sl_status_t sl_se_gcm_crypt_and_tag | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
size_t | length, |
||
const unsigned char * | iv, |
||
size_t | iv_len, |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
size_t | tag_len, |
||
unsigned char * | tag |
||
) |
This function performs GCM encryption or decryption of a buffer.
- Note
- For encryption, the output buffer can be the same as the input buffer. For decryption, the output buffer cannot be the same as input buffer. If the buffers overlap, the output buffer must trail at least 8 bytes behind the input buffer.
- Warning
- When this function performs a decryption, it outputs the authentication tag and does not verify that the data is authentic. You should use this function to perform encryption only. For decryption, use sl_se_gcm_auth_decrypt() instead.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] mode
Crypto operation type (encryption or decryption). - SL_SE_ENCRYPT: The ciphertext is written to
output
and the authentication tag is written totag
. - SL_SE_DECRYPT: The plaintext is written to
output
and the authentication tag is written totag
. Note that this mode is not recommended, because it does not verify the authenticity of the data. For this reason, you should use sl_se_gcm_auth_decrypt() instead.
[in] length
The length of the input data, which is equal to the length of the output data. [in] iv
The initialization vector. [in] iv_len
The length of the iv. Must be 12 bytes. [in] add
The buffer holding the additional data. [in] add_len
The length of the additional data in bytes. [in] input
The buffer holding the input data. Its size is length bytes. [out] output
The buffer for holding the output data. It must have room for length bytes. [in] tag_len
The length of the tag to generate (in bytes). [out] tag
The buffer for holding the tag. - SL_SE_ENCRYPT: The ciphertext is written to
- Returns
- SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
◆ sl_se_gcm_auth_decrypt()
sl_status_t sl_se_gcm_auth_decrypt | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char * | iv, |
||
size_t | iv_len, |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
size_t | tag_len, |
||
const unsigned char * | tag |
||
) |
This function performs a GCM authenticated decryption of a buffer.
- Note
- The output buffer cannot be the same as input buffer. If the buffers overlap, the output buffer must trail at least 8 bytes behind the input buffer.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
The length of the ciphertext to decrypt, which is also the length of the decrypted plaintext. [in] iv
The initialization vector. [in] iv_len
The length of the iv. Must be 12 bytes. [in] add
The buffer holding the additional data. [in] add_len
The length of the additional data in bytes. [in] tag
The buffer holding the tag to verify. [in] tag_len
The length of the tag to verify (in bytes). [in] input
The buffer holding the ciphertext. Its size is length bytes. [out] output
The buffer for holding the decrypted plaintext. It must have room for length bytes.
- Returns
- SL_STATUS_OK when the command was executed successfully, otherwise an appropriate error code (sl_status.h).
◆ sl_se_cmac()
sl_status_t sl_se_cmac | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
const unsigned char * | input, |
||
size_t | input_len, |
||
unsigned char * | output |
||
) |
This function calculates the full generic CMAC on the input buffer with the provided key.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] input
Buffer holding the input data, must be at least input_len
bytes wide.[in] input_len
The length of the input data in bytes. [out] output
Buffer holding the 16-byte output data, must be at least 16 bytes wide.
- Returns
- Status code, sl_status.h.
◆ sl_se_cmac_starts()
sl_status_t sl_se_cmac_starts | ( | sl_se_cmac_streaming_context_t * | cmac_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
const sl_se_key_descriptor_t * | key |
||
) |
Prepare a CMAC streaming command context object.
Prepare a CMAC streaming command context object to be used in subsequent CMAC streaming function calls.
- Parameters
-
[in] cmac_ctx
Pointer to a CMAC streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure.
- Returns
- Status code, sl_status.h.
◆ sl_se_cmac_update()
sl_status_t sl_se_cmac_update | ( | sl_se_cmac_streaming_context_t * | cmac_ctx, |
const uint8_t * | input, |
||
size_t | input_len |
||
) |
This function feeds an input buffer into an ongoing CMAC computation.
It is called between sl_se_cmac_starts() and sl_se_cmac_finish(). Can be called repeatedly.
- Parameters
-
[in,out] cmac_ctx
Pointer to a CMAC streaming context object. [in] input
Buffer holding the input data, must be at least input_len
bytes wide.[in] input_len
The length of the input data in bytes.
- Returns
- Status code, sl_status.h.
◆ sl_se_cmac_finish()
sl_status_t sl_se_cmac_finish | ( | sl_se_cmac_streaming_context_t * | cmac_ctx, |
uint8_t * | output |
||
) |
Finish a CMAC streaming operation and return the resulting CMAC tag.
It is called after sl_se_cmac_update().
- Parameters
-
[in,out] cmac_ctx
Pointer to a CMAC streaming context object. [out] output
Buffer holding the 16-byte CMAC tag, must be at least 16 bytes wide.
- Returns
- Status code, sl_status.h.
◆ sl_se_gcm_starts()
sl_status_t sl_se_gcm_starts | ( | sl_se_gcm_streaming_context_t * | gcm_ctx, |
sl_se_command_context_t * | cmd_ctx, |
||
const sl_se_key_descriptor_t * | key, |
||
sl_se_cipher_operation_t | mode, |
||
const uint8_t * | iv, |
||
size_t | iv_len, |
||
const uint8_t * | add, |
||
size_t | add_len |
||
) |
Prepare a GCM streaming command context object.
Prepare a GCM streaming command context object to be used in subsequent GCM streaming function calls.
- Parameters
-
[in] gcm_ctx
Pointer to a GCM streaming context object. [in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. mode
The operation to perform: SL_SE_ENCRYPT or SL_SE_DECRYPT. iv
The initialization vector. iv_len
The length of the IV. add
The buffer holding the additional data, or NULL if add_len
is 0.add_len
The length of the additional data. If 0, add
is NULL.
- Returns
- Status code, sl_status.h.
◆ sl_se_gcm_update()
sl_status_t sl_se_gcm_update | ( | sl_se_gcm_streaming_context_t * | gcm_ctx, |
size_t | length, |
||
const uint8_t * | input, |
||
uint8_t * | output |
||
) |
This function feeds an input buffer into an ongoing GCM computation.
It is called between sl_se_gcm_starts() and sl_se_gcm_finish(). Can be called repeatedly.
- Parameters
-
[in] gcm_ctx
Pointer to a GCM streaming context object. [in] length
The length of the input data. This must be a multiple of 16 except in the last call before sl_se_gcm_finish(). [in] input
Buffer holding the input data, must be at least length
bytes wide.[out] output
Buffer for holding the output data, must be at least length
bytes wide.
- Returns
- Status code, sl_status.h.
◆ sl_se_gcm_finish()
sl_status_t sl_se_gcm_finish | ( | sl_se_gcm_streaming_context_t * | gcm_ctx, |
uint8_t * | tag, |
||
size_t | tag_len |
||
) |
Finish a GCM streaming operation and return the resulting GCM tag.
It is called after sl_se_gcm_update().
- Parameters
-
[in] gcm_ctx
Pointer to a GCM streaming context object. [out] tag
The buffer for holding the tag. [in] tag_len
The length of the tag to generate. Must be at least four.
- Returns
- Status code, sl_status.h.
◆ sl_se_hmac()
sl_status_t sl_se_hmac | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
sl_se_hash_type_t | hash_type, |
||
const uint8_t * | message, |
||
size_t | message_len, |
||
uint8_t * | output, |
||
size_t | output_len |
||
) |
Compute a HMAC on a full message.
This function computes a Keyed-Hashed Message Authentication Code (HMAC) for the given input message. HMAC can be used with any iterative cryptographic hash function, e.g., SHA-1 in combination with a secret shared key. The cryptographic strength of HMAC depends on the properties of the underlying hash function. For instance, if the algorithm is chosen to be SHA-256, it will generate a 32 bytes HMAC. This function supports SHA-1, SHA-224, SHA-256, SHA-384 and SHA-512. The key can be of any length. If the key is shorter than the block size of the hash function the SE will append zeros to the key so the key size matches the block size of the hash function. If the key is longer than the block size of the hash function the key will be hashed to produce a key digest, then append zeros so the resulting 'hashed' key size matches the block size of the hash function. In any case the minimal recommended key length is the digest size of the hash function.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure specifying the key to use in the HMAC computation. [in] hash_type
Which hashing algorithm to use. [in] message
Pointer to the message buffer to compute the hash/digest from. [in] message_len
Number of bytes in message. [out] output
Pointer to memory buffer to store the final HMAC output. [in] output_len
The length of the HMAC output memory buffer, must be at least the size of the corresponding hash type.
- Returns
- Status code, sl_status.h.
◆ sl_se_chacha20_crypt()
sl_status_t sl_se_chacha20_crypt | ( | sl_se_command_context_t * | cmd_ctx, |
sl_se_cipher_operation_t | mode, |
||
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char | initial_counter[4], |
||
const unsigned char | nonce[12], |
||
const unsigned char * | input, |
||
unsigned char * | output |
||
) |
ChaCha20 buffer encryption/decryption, as defined by RFC8439 section 2.4.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] mode
Crypto operation type (encryption or decryption). [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
Length of the input data. [in] initial_counter
The initial counter value as defined in RFC8439 section 2.4. [in] nonce
The nonce, also called initialisation vector, as defined in RFC8439 section 2.4. [in] input
Buffer holding the input data. [out] output
Buffer holding the output data.
- Returns
- Status code, sl_status.h.
◆ sl_se_chacha20_poly1305_encrypt_and_tag()
sl_status_t sl_se_chacha20_poly1305_encrypt_and_tag | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char | nonce[12], |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
unsigned char * | tag |
||
) |
ChaCha20-Poly1305 authenticated encryption with additional data, as defined by RFC8439 section 2.8.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
The length of the input data in bytes. [in] nonce
The nonce, also called initialisation vector, as defined in RFC8439 section 2.8. [in] add
The buffer holding additional authenticated data. Can be NULL if add_len
equals 0.[in] add_len
The length of the additional authenticated data in bytes. [in] input
The buffer holding the plaintext input. [out] output
The buffer holding the ciphertext output. Can be NULL, in which case the generated ciphertext will be discarded. Must be at least length
bytes wide.[out] tag
The buffer holding the tag. This function will produce a 128-bit tag, so this buffer must be at least 16 bytes wide. Can be NULL, in which case the generated tag will be discarded.
- Returns
- Status code, sl_status.h.
◆ sl_se_chacha20_poly1305_auth_decrypt()
sl_status_t sl_se_chacha20_poly1305_auth_decrypt | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char | nonce[12], |
||
const unsigned char * | add, |
||
size_t | add_len, |
||
const unsigned char * | input, |
||
unsigned char * | output, |
||
const unsigned char | tag[16] |
||
) |
ChaCha20-Poly1305 authenticated decryption with additional data, as defined by RFC8439 section 2.8.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure. [in] length
The length of the input data in Bytes. [in] nonce
The nonce, also called initialisation vector, as defined in RFC8439 section 2.8. [in] add
The buffer holding additional authenticated data. Can be NULL if add_len
equals 0.[in] add_len
The length of the additional authenticated data in bytes. [in] input
The buffer holding the ciphertext to decrypt. Can be NULL if length
equals 0.[out] output
The buffer holding the plaintext output. Can be NULL, in which case the decrypted plaintext will be discarded, or when length
equals 0. Must be at leastlength
bytes wide.[in] tag
The buffer holding the tag to verify.
- Returns
- Status code, sl_status.h.
◆ sl_se_poly1305_genkey_tag()
sl_status_t sl_se_poly1305_genkey_tag | ( | sl_se_command_context_t * | cmd_ctx, |
const sl_se_key_descriptor_t * | key, |
||
size_t | length, |
||
const unsigned char | nonce[12], |
||
const unsigned char * | input, |
||
unsigned char * | tag |
||
) |
Generate a Poly1305 MAC (message authentication code) for a given message using an ephemeral key derived using ChaCha20.
- Note
- This function first derives a Poly1305 key based on a ChaCha20 key and nonce, which are input to this function. The key derivation adheres to RFC8439 section 2.6. The derived key is then used to calculate a MAC of the input data, according to RFC8439 section 2.5.
- Parameters
-
[in] cmd_ctx
Pointer to an SE command context object. [in] key
Pointer to sl_se_key_descriptor_t structure containing a ChaCha20 key. [in] length
The length of the input data in Bytes. [in] nonce
The nonce, also called initialisation vector, as defined in RFC8439 section 2.6. [in] input
The buffer holding the input data. [out] tag
The buffer holding the tag. This function will produce a 128-bit tag, so this buffer must be at least 16 bytes wide.
- Returns
- Status code, sl_status.h.
Macro Definition Documentation
◆ SL_SE_CMAC_STREAMING_INIT_DEFAULT
#define SL_SE_CMAC_STREAMING_INIT_DEFAULT { NULL, { 0 }, { 0 }, 0 } |
Initial values for CMAC streaming context struct sl_se_cmac_streaming_context_t.
◆ SL_SE_GCM_STREAMING_INIT_DEFAULT
#define SL_SE_GCM_STREAMING_INIT_DEFAULT |
Initial values for AES-GCM streaming context struct sl_se_gcm_streaming_context_t.
Enumeration Type Documentation
◆ sl_se_cipher_operation_t
Cipher operation types.