IO Stream STDLIB Configuration
Description
IO Stream STDLIB Configuration.
Overview
The buffering mode is enabled by default in nano-lib meaning that the low-level write function is called only when a '
' is seen by the standard library. This module allows to disable the buffering feature and output the data as soon as possible.
Functions | |
void | sl_iostream_stdlib_disable_buffering (void) |
Disable standard library buffering. | |
Function Documentation
◆ sl_iostream_stdlib_disable_buffering()
void sl_iostream_stdlib_disable_buffering | ( | void |
| ) |
Disable standard library buffering.