VCMP - Voltage Comparator
Description
Supply Voltage Comparator (VCMP) Peripheral API.
This module contains functions to control the VCMP peripheral of Silicon Labs 32-bit MCUs and SoCs. The VCMP monitors the input voltage supply and generates interrupts on events using as little as 100 nA.
Data Structures | |
struct | VCMP_Init_TypeDef |
VCMP Initialization structure. | |
Functions | |
void | VCMP_Init (const VCMP_Init_TypeDef *vcmpInit) |
Configure and enable Voltage Comparator. | |
void | VCMP_LowPowerRefSet (bool enable) |
Enable or disable Low Power Reference setting. | |
void | VCMP_TriggerSet (int level) |
Configure the trigger level of the voltage comparator. | |
void | VCMP_Enable (void) |
Enable Voltage Comparator. | |
void | VCMP_Disable (void) |
Disable Voltage Comparator. | |
uint32_t | VCMP_VoltageToLevel (float v) |
Calculate voltage to trigger level. | |
bool | VCMP_VDDLower (void) |
Check if VDD is lower than trigger level. | |
bool | VCMP_VDDHigher (void) |
Check if VDD is higher than trigger level. | |
bool | VCMP_Ready (void) |
Check if VCMP output is ready. | |
void | VCMP_IntClear (uint32_t flags) |
Clear one or more pending VCMP interrupts. | |
void | VCMP_IntSet (uint32_t flags) |
Set one or more pending VCMP interrupts from SW. | |
void | VCMP_IntDisable (uint32_t flags) |
Disable one or more VCMP interrupts. | |
void | VCMP_IntEnable (uint32_t flags) |
Enable one or more VCMP interrupts. | |
uint32_t | VCMP_IntGet (void) |
Get pending VCMP interrupt flags. | |
uint32_t | VCMP_IntGetEnabled (void) |
Get enabled and pending VCMP interrupt flags. | |
Macros | |
#define | VCMP_INIT_DEFAULT |
Default VCMP initialization structure. | |
Enumerations | |
enum | VCMP_WarmTime_TypeDef { vcmpWarmTime4Cycles = _VCMP_CTRL_WARMTIME_4CYCLES, vcmpWarmTime8Cycles = _VCMP_CTRL_WARMTIME_8CYCLES, vcmpWarmTime16Cycles = _VCMP_CTRL_WARMTIME_16CYCLES, vcmpWarmTime32Cycles = _VCMP_CTRL_WARMTIME_32CYCLES, vcmpWarmTime64Cycles = _VCMP_CTRL_WARMTIME_64CYCLES, vcmpWarmTime128Cycles = _VCMP_CTRL_WARMTIME_128CYCLES, vcmpWarmTime256Cycles = _VCMP_CTRL_WARMTIME_256CYCLES, vcmpWarmTime512Cycles = _VCMP_CTRL_WARMTIME_512CYCLES } |
Warm-up Time in High Frequency Peripheral Clock cycles. | |
enum | VCMP_Hysteresis_TypeDef { vcmpHystNone, vcmpHyst20mV } |
Hysteresis configuration. | |
Function Documentation
◆ VCMP_Init()
void VCMP_Init | ( | const VCMP_Init_TypeDef * | vcmpInit | ) |
Configure and enable Voltage Comparator.
- Parameters
-
[in] vcmpInit
The VCMP Initialization structure.
◆ VCMP_LowPowerRefSet()
void VCMP_LowPowerRefSet | ( | bool | enable | ) |
Enable or disable Low Power Reference setting.
- Parameters
-
[in] enable
If true, enables low power reference. If false, disable low power reference.
◆ VCMP_TriggerSet()
void VCMP_TriggerSet | ( | int | level | ) |
Configure the trigger level of the voltage comparator.
- Parameters
-
[in] level
A trigger value, in range 0-63.
◆ VCMP_Enable()
|
inline |
Enable Voltage Comparator.
◆ VCMP_Disable()
|
inline |
Disable Voltage Comparator.
◆ VCMP_VoltageToLevel()
|
inline |
Calculate voltage to trigger level.
- Note
- Soft float support is needed for this function to work.
- Parameters
-
[in] v
Voltage Level for trigger.
- Returns
- Trigger level.
◆ VCMP_VDDLower()
|
inline |
Check if VDD is lower than trigger level.
- Returns
- True if Voltage Comparator indicated VDD < trigger level, else returns false.
◆ VCMP_VDDHigher()
|
inline |
Check if VDD is higher than trigger level.
- Returns
- True if Voltage Comparator indicated VDD > trigger level, else returns false.
◆ VCMP_Ready()
|
inline |
Check if VCMP output is ready.
- Returns
- True if VCMP output is ready.
◆ VCMP_IntClear()
|
inline |
Clear one or more pending VCMP interrupts.
- Parameters
-
[in] flags
VCMP interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
◆ VCMP_IntSet()
|
inline |
Set one or more pending VCMP interrupts from SW.
- Parameters
-
[in] flags
VCMP interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
◆ VCMP_IntDisable()
|
inline |
Disable one or more VCMP interrupts.
- Parameters
-
[in] flags
VCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
◆ VCMP_IntEnable()
|
inline |
Enable one or more VCMP interrupts.
- Parameters
-
[in] flags
VCMP interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the VCMP module (VCMP_IFS_nnn).
◆ VCMP_IntGet()
|
inline |
Get pending VCMP interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending VCMP interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the VCMP module (VCMP_IFS_nnn).
◆ VCMP_IntGetEnabled()
|
inline |
Get enabled and pending VCMP interrupt flags.
Useful for handling more interrupt sources in the same interrupt handler.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- Pending and enabled VCMP interrupt sources. The return value is the bitwise AND combination of
- the OR combination of enabled interrupt sources in VCMP_IEN_nnn register (VCMP_IEN_nnn) and
- the OR combination of valid interrupt flags of the VCMP module (VCMP_IF_nnn).
Macro Definition Documentation
◆ VCMP_INIT_DEFAULT
#define VCMP_INIT_DEFAULT |
Default VCMP initialization structure.
Enumeration Type Documentation
◆ VCMP_WarmTime_TypeDef
Warm-up Time in High Frequency Peripheral Clock cycles.