ACMP_Init_TypeDef Struct Reference
ACMP initialization structure.
#include <em_acmp.h>
Data Fields |
|
bool | fullBias |
Full-bias current.
|
|
bool | halfBias |
Half-bias current.
|
|
uint32_t | biasProg |
Bias current.
|
|
bool | interruptOnFallingEdge |
Enable setting the interrupt flag on the falling edge.
|
|
bool | interruptOnRisingEdge |
Enable setting the interrupt flag on the rising edge.
|
|
ACMP_WarmTime_TypeDef | warmTime |
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
|
|
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
Hysteresis level.
|
|
bool | inactiveValue |
Inactive value emitted by ACMP during warmup.
|
|
bool | lowPowerReferenceEnabled |
Low power reference enabled.
|
|
uint32_t | vddLevel |
VDD reference value.
|
|
bool | enable |
If true, ACMP is enabled after configuration.
|
|
ACMP initialization structure.
Field Documentation
◆ fullBias
bool ACMP_Init_TypeDef::fullBias |
Full-bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ halfBias
bool ACMP_Init_TypeDef::halfBias |
Half-bias current.
See the ACMP chapter about bias and response time in the reference manual for details.
◆ biasProg
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current.
See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
◆ interruptOnFallingEdge
bool ACMP_Init_TypeDef::interruptOnFallingEdge |
Enable setting the interrupt flag on the falling edge.
◆ interruptOnRisingEdge
bool ACMP_Init_TypeDef::interruptOnRisingEdge |
Enable setting the interrupt flag on the rising edge.
◆ warmTime
ACMP_WarmTime_TypeDef ACMP_Init_TypeDef::warmTime |
Warmup time, which is measured in HFPERCLK / HFPERCCLK cycles and should be about 10 us in wall clock time.
◆ hysteresisLevel
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
Hysteresis level.
◆ inactiveValue
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
◆ lowPowerReferenceEnabled
bool ACMP_Init_TypeDef::lowPowerReferenceEnabled |
Low power reference enabled.
This setting, if enabled, reduces the power used by the VDD and bandgap references.
◆ vddLevel
uint32_t ACMP_Init_TypeDef::vddLevel |
VDD reference value.
VDD_SCALED = VDD * VDDLEVEL * 50 mV/3.8 V. Valid values are in the 0-63 range.
◆ enable
bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.