WDOG_Init_TypeDef Struct Reference
Watchdog initialization structure.
      
       #include <em_wdog.h>
      
     
| Data Fields | |
| bool | enable | 
| Enable watchdog when initialization completed. | |
| bool | debugRun | 
| Counter keeps running during debug halt. | |
| bool | em2Run | 
| Counter keeps running when in EM2. | |
| bool | em3Run | 
| Counter keeps running when in EM3. | |
| bool | em4Block | 
| Block EMU from entering EM4. | |
| bool | swoscBlock | 
| Block SW from disabling LFRCO/LFXO oscillators. | |
| bool | lock | 
| Block SW from modifying the configuration (a reset is needed to reconfigure). | |
| WDOG_ClkSel_TypeDef | clkSel | 
| Clock source to use for watchdog. | |
| WDOG_PeriodSel_TypeDef | perSel | 
| Watchdog timeout period. | |
Watchdog initialization structure.
Field Documentation
◆ enable
| bool WDOG_Init_TypeDef::enable | 
Enable watchdog when initialization completed.
◆ debugRun
| bool WDOG_Init_TypeDef::debugRun | 
Counter keeps running during debug halt.
◆ em2Run
| bool WDOG_Init_TypeDef::em2Run | 
Counter keeps running when in EM2.
◆ em3Run
| bool WDOG_Init_TypeDef::em3Run | 
Counter keeps running when in EM3.
◆ em4Block
| bool WDOG_Init_TypeDef::em4Block | 
Block EMU from entering EM4.
◆ swoscBlock
| bool WDOG_Init_TypeDef::swoscBlock | 
Block SW from disabling LFRCO/LFXO oscillators.
◆ lock
| bool WDOG_Init_TypeDef::lock | 
Block SW from modifying the configuration (a reset is needed to reconfigure).
◆ clkSel
| WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel | 
Clock source to use for watchdog.
◆ perSel
| WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel | 
Watchdog timeout period.