EBI - External Bus Interface

Description

EBI External Bus Interface (EBI) Peripheral API.

This module contains functions to control the EBI peripheral of Silicon Labs 32-bit MCUs and SoCs. The EBI is used for accessing external parallel devices. The devices appear as part of the internal memory map of the MCU.

Data Structures

struct EBI_Init_TypeDef
EBI Initialization structure.
struct EBI_TFTInit_TypeDef
TFT Initialization structure.

Functions

void EBI_Init (const EBI_Init_TypeDef *ebiInit)
Configure and enable the External Bus Interface.
void EBI_Disable (void)
Disable External Bus Interface.
void EBI_BankEnable (uint32_t banks, bool enable)
Enable or disable EBI Bank.
uint32_t EBI_BankAddress (uint32_t bank)
Return the base address of the EBI bank.
void EBI_NANDFlashEnable (uint32_t banks, bool enable)
Enable or disable EBI NAND Flash Support.
void EBI_ChipSelectEnable (uint32_t cs, bool enable)
Enable or disable EBI Chip Select.
void EBI_PolaritySet ( EBI_Line_TypeDef line, EBI_Polarity_TypeDef polarity)
Configure EBI pin polarity.
void EBI_ReadTimingSet (uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles)
Configure timing values of read bus accesses.
void EBI_WriteTimingSet (uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles)
Configure timing values of write bus accesses.
void EBI_AddressTimingSet (uint32_t setupCycles, uint32_t holdCycles)
Configure timing values of address latch bus accesses.
void EBI_TFTInit (const EBI_TFTInit_TypeDef *ebiTFTInit)
Configure and initialize TFT Direct Drive.
void EBI_TFTSizeSet (uint32_t horizontal, uint32_t vertical)
Configure and initialize TFT size settings.
void EBI_TFTHPorchSet (uint32_t front, uint32_t back, uint32_t pulseWidth)
Configure and initialize Horizontal Porch Settings.
void EBI_TFTVPorchSet (uint32_t front, uint32_t back, uint32_t pulseWidth)
Configure Vertical Porch Settings.
void EBI_TFTTimingSet (uint32_t dclkPeriod, uint32_t start, uint32_t setup, uint32_t hold)
Configure TFT Direct Drive Timing Settings.
void EBI_BankReadTimingConfig (uint32_t banks, bool pageMode, bool prefetch, bool halfRE)
Configure read operation parameters for a selected bank.
void EBI_BankReadTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles)
Configure timing values of read bus accesses.
void EBI_BankWriteTimingConfig (uint32_t banks, bool writeBufDisable, bool halfWE)
Configure write operation parameters for a selected bank.
void EBI_BankWriteTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t strobeCycles, uint32_t holdCycles)
Configure timing values of write bus accesses.
void EBI_BankAddressTimingConfig (uint32_t banks, bool halfALE)
Configure address operation parameters for a selected bank.
void EBI_BankAddressTimingSet (uint32_t banks, uint32_t setupCycles, uint32_t holdCycles)
Configure timing values of address latch bus accesses.
void EBI_BankPolaritySet (uint32_t banks, EBI_Line_TypeDef line, EBI_Polarity_TypeDef polarity)
Configure EBI pin polarity for selected bank(s) for devices with individual timing support.
void EBI_BankByteLaneEnable (uint32_t banks, bool enable)
Configure Byte Lane Enable for select banks timing support.
void EBI_AltMapEnable (bool enable)
Configure the Alternate Address Map support.
void EBI_TFTEnable ( EBI_TFTDDMode_TypeDef mode)
Enable or disable TFT Direct Drive.
void EBI_TFTFrameBaseSet (uint32_t address)
Configure frame buffer pointer.
void EBI_TFTPixelSet (int pixel, uint32_t color)
Set TFT Pixel Color 0 or 1.
void EBI_TFTDDSet (uint32_t color)
Set TFT Direct Drive Data from Internal Memory.
void EBI_TFTColorFormatSet ( EBI_TFTColorFormat_TypeDef color0, EBI_TFTColorFormat_TypeDef color1)
Set TFT Color Format.
void EBI_TFTMaskBlendMode ( EBI_TFTMaskBlend_TypeDef maskBlend)
Masking and Blending Mode Set.
void EBI_TFTColorSrcSet ( EBI_TFTColorSrc_TypeDef colorSrc)
Masking and Blending Color1 Source Set.
void EBI_TFTAlphaBlendSet (uint8_t alpha)
Set TFT Alpha Blending Factor.
void EBI_TFTMaskSet (uint32_t mask)
Set TFT mask value.
uint32_t EBI_TFTVCount (void)
Get current vertical position counter.
uint32_t EBI_TFTHCount (void)
Get current horizontal position counter.
void EBI_TFTFBTriggerSet ( EBI_TFTFrameBufTrigger_TypeDef sync)
Set Frame Buffer Trigger.
void EBI_TFTHStrideSet (uint32_t nbytes)
Set horizontal TFT stride value in number of bytes.
void EBI_IntClear (uint32_t flags)
Clear one or more pending EBI interrupts.
void EBI_IntSet (uint32_t flags)
Set one or more pending EBI interrupts.
void EBI_IntDisable (uint32_t flags)
Disable one or more EBI interrupts.
void EBI_IntEnable (uint32_t flags)
Enable one or more EBI interrupts.
uint32_t EBI_IntGet (void)
Get pending EBI interrupt flags.
uint32_t EBI_IntGetEnabled (void)
Get enabled and pending EBI interrupt flags.
void EBI_StartNandEccGen (void)
Start ECC generator on NAND flash transfers.
uint32_t EBI_StopNandEccGen (void)
Stop NAND flash ECC generator and return generated ECC.

Macros

#define EBI_BANK0 (uint32_t)(1 << 1)
EBI address bank 0.
#define EBI_BANK1 (uint32_t)(1 << 2)
EBI address bank 1.
#define EBI_BANK2 (uint32_t)(1 << 3)
EBI address bank 2.
#define EBI_BANK3 (uint32_t)(1 << 4)
EBI address bank 3.
#define EBI_CS0 (uint32_t)(1 << 1)
EBI chip select line 0.
#define EBI_CS1 (uint32_t)(1 << 2)
EBI chip select line 1.
#define EBI_CS2 (uint32_t)(1 << 3)
EBI chip select line 2.
#define EBI_CS3 (uint32_t)(1 << 4)
EBI chip select line 3.
#define EBI_GENERIC_ALB_A0 EBI_ROUTEPEN_ALB_A0
Pin Enable Lower Bound EBI_A[0] and upwards.
#define EBI_GENERIC_ALB_A8 EBI_ROUTEPEN_ALB_A8
Pin Enable Lower Bound EBI_A[8] and upwards.
#define EBI_GENERIC_ALB_A16 EBI_ROUTEPEN_ALB_A16
Pin Enable Lower Bound EBI_A[16] and upwards.
#define EBI_GENERIC_ALB_A24 EBI_ROUTEPEN_ALB_A24
Pin Enable Lower Bound EBI_A[24] and upwards.
#define EBI_GENERIC_APEN_A0 EBI_ROUTEPEN_APEN_A0
All EBI_A pins enabled.
#define EBI_GENERIC_APEN_A5 EBI_ROUTEPEN_APEN_A5
EBI_A[4:L] pins enabled.
#define EBI_GENERIC_APEN_A6 EBI_ROUTEPEN_APEN_A6
EBI_A[5:L] pins enabled.
#define EBI_GENERIC_APEN_A7 EBI_ROUTEPEN_APEN_A7
EBI_A[6:L] pins enabled.
#define EBI_GENERIC_APEN_A8 EBI_ROUTEPEN_APEN_A8
EBI_A[7:L] pins enabled.
#define EBI_GENERIC_APEN_A9 EBI_ROUTEPEN_APEN_A9
EBI_A[8:L] pins enabled.
#define EBI_GENERIC_APEN_A10 EBI_ROUTEPEN_APEN_A10
EBI_A[9:L] pins enabled.
#define EBI_GENERIC_APEN_A11 EBI_ROUTEPEN_APEN_A11
EBI_A[10:L] pins enabled.
#define EBI_GENERIC_APEN_A12 EBI_ROUTEPEN_APEN_A12
EBI_A[11:L] pins enabled.
#define EBI_GENERIC_APEN_A13 EBI_ROUTEPEN_APEN_A13
EBI_A[12:L] pins enabled.
#define EBI_GENERIC_APEN_A14 EBI_ROUTEPEN_APEN_A14
EBI_A[13:L] pins enabled.
#define EBI_GENERIC_APEN_A15 EBI_ROUTEPEN_APEN_A15
EBI_A[14:L] pins enabled.
#define EBI_GENERIC_APEN_A16 EBI_ROUTEPEN_APEN_A16
EBI_A[15:L] pins enabled.
#define EBI_GENERIC_APEN_A17 EBI_ROUTEPEN_APEN_A17
EBI_A[16:L] pins enabled.
#define EBI_GENERIC_APEN_A18 EBI_ROUTEPEN_APEN_A18
EBI_A[17:L] pins enabled.
#define EBI_GENERIC_APEN_A19 EBI_ROUTEPEN_APEN_A19
EBI_A[18:L] pins enabled.
#define EBI_GENERIC_APEN_A20 EBI_ROUTEPEN_APEN_A20
EBI_A[19:L] pins enabled.
#define EBI_GENERIC_APEN_A21 EBI_ROUTEPEN_APEN_A21
EBI_A[20:L] pins enabled.
#define EBI_GENERIC_APEN_A22 EBI_ROUTEPEN_APEN_A22
EBI_A[21:L] pins enabled.
#define EBI_GENERIC_APEN_A23 EBI_ROUTEPEN_APEN_A23
EBI_A[22:L] pins enabled.
#define EBI_GENERIC_APEN_A24 EBI_ROUTEPEN_APEN_A24
EBI_A[23:L] pins enabled.
#define EBI_GENERIC_APEN_A25 EBI_ROUTEPEN_APEN_A25
EBI_A[24:L] pins enabled.
#define EBI_GENERIC_APEN_A26 EBI_ROUTEPEN_APEN_A26
EBI_A[25:L] pins enabled.
#define EBI_GENERIC_APEN_A27 EBI_ROUTEPEN_APEN_A27
EBI_A[26:L] pins enabled.
#define EBI_GENERIC_APEN_A28 EBI_ROUTEPEN_APEN_A28
EBI_A[27:L] pins enabled.
#define EBI_INIT_DEFAULT
Default configuration for EBI initialization structures.
#define EBI_TFTINIT_DEFAULT
Default configuration for EBI TFT initialization structure.

Enumerations

enum EBI_Mode_TypeDef {
ebiModeD8A8 = EBI_CTRL_MODE_D8A8,
ebiModeD16A16ALE = EBI_CTRL_MODE_D16A16ALE,
ebiModeD8A24ALE = EBI_CTRL_MODE_D8A24ALE,
ebiModeD16 = EBI_CTRL_MODE_D16
}
EBI Mode of operation.
enum EBI_Polarity_TypeDef {
ebiActiveLow = 0,
ebiActiveHigh = 1
}
EBI Polarity configuration.
enum EBI_Line_TypeDef {
ebiLineARDY ,
ebiLineALE ,
ebiLineWE ,
ebiLineRE ,
ebiLineCS ,
ebiLineBL ,
ebiLineTFTVSync ,
ebiLineTFTHSync ,
ebiLineTFTDataEn ,
ebiLineTFTDClk ,
ebiLineTFTCS
}
EBI Pin Line types.
enum EBI_ALow_TypeDef {
ebiALowA0 = EBI_GENERIC_ALB_A0,
ebiALowA8 = EBI_GENERIC_ALB_A8,
ebiALowA16 = EBI_GENERIC_ALB_A16,
ebiALowA24 = EBI_GENERIC_ALB_A24
}
Address Pin Enable, lower limit - lower range of pins to enable.
enum EBI_AHigh_TypeDef {
ebiAHighA0 = EBI_GENERIC_APEN_A0,
ebiAHighA5 = EBI_GENERIC_APEN_A5,
ebiAHighA6 = EBI_GENERIC_APEN_A6,
ebiAHighA7 = EBI_GENERIC_APEN_A7,
ebiAHighA8 = EBI_GENERIC_APEN_A8,
ebiAHighA9 = EBI_GENERIC_APEN_A9,
ebiAHighA10 = EBI_GENERIC_APEN_A10,
ebiAHighA11 = EBI_GENERIC_APEN_A11,
ebiAHighA12 = EBI_GENERIC_APEN_A12,
ebiAHighA13 = EBI_GENERIC_APEN_A13,
ebiAHighA14 = EBI_GENERIC_APEN_A14,
ebiAHighA15 = EBI_GENERIC_APEN_A15,
ebiAHighA16 = EBI_GENERIC_APEN_A16,
ebiAHighA17 = EBI_GENERIC_APEN_A17,
ebiAHighA18 = EBI_GENERIC_APEN_A18,
ebiAHighA19 = EBI_GENERIC_APEN_A19,
ebiAHighA20 = EBI_GENERIC_APEN_A20,
ebiAHighA21 = EBI_GENERIC_APEN_A21,
ebiAHighA22 = EBI_GENERIC_APEN_A22,
ebiAHighA23 = EBI_GENERIC_APEN_A23,
ebiAHighA24 = EBI_GENERIC_APEN_A24,
ebiAHighA25 = EBI_GENERIC_APEN_A25,
ebiAHighA26 = EBI_GENERIC_APEN_A26,
ebiAHighA27 = EBI_GENERIC_APEN_A27,
ebiAHighA28 = EBI_GENERIC_APEN_A28
}
Address Pin Enable, high limit - higher limit of pins to enable.
enum EBI_TFTBank_TypeDef {
ebiTFTBank0 = EBI_TFTCTRL_BANKSEL_BANK0,
ebiTFTBank1 = EBI_TFTCTRL_BANKSEL_BANK1,
ebiTFTBank2 = EBI_TFTCTRL_BANKSEL_BANK2,
ebiTFTBank3 = EBI_TFTCTRL_BANKSEL_BANK3
}
EBI TFT Graphics Bank Select.
enum EBI_TFTColorFormat_TypeDef {
ebiTFTARGB0555 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0555,
ebiTFTARGB0565 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0565,
ebiTFTARGB0666 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0666,
ebiTFTARGB0888 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB0888,
ebiTFTARGB5555 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB5555,
ebiTFTARGB6565 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB6565,
ebiTFTARGB6666 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB6666,
ebiTFTARGB8888 = EBI_TFTCOLORFORMAT_PIXEL0FORMAT_ARGB8888,
ebiTFTRGB555 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB555,
ebiTFTRGB565 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB565,
ebiTFTRGB666 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB666,
ebiTFTRGB888 = EBI_TFTCOLORFORMAT_PIXEL1FORMAT_RGB888
}
EBI TFT Color format.
enum EBI_TFTColorSrc_TypeDef {
ebiTFTColorSrcMem = EBI_TFTCTRL_COLOR1SRC_MEM,
ebiTFTColorSrcPixel1 = EBI_TFTCTRL_COLOR1SRC_PIXEL1
}
Masking and Alpha blending source color.
enum EBI_TFTInterleave_TypeDef {
ebiTFTInterleaveUnlimited = EBI_TFTCTRL_INTERLEAVE_UNLIMITED,
ebiTFTInterleaveOnePerDClk = EBI_TFTCTRL_INTERLEAVE_ONEPERDCLK,
ebiTFTInterleavePorch = EBI_TFTCTRL_INTERLEAVE_PORCH
}
Bus Data Interleave Mode.
enum EBI_TFTFrameBufTrigger_TypeDef {
ebiTFTFrameBufTriggerVSync = EBI_TFTCTRL_FBCTRIG_VSYNC,
ebiTFTFrameBufTriggerHSync = EBI_TFTCTRL_FBCTRIG_HSYNC
}
Control frame base pointer copy.
enum EBI_TFTMaskBlend_TypeDef {
ebiTFTMBDisabled = EBI_TFTCTRL_MASKBLEND_DISABLED,
ebiTFTMBIMask = EBI_TFTCTRL_MASKBLEND_IMASK,
ebiTFTMBIAlpha = EBI_TFTCTRL_MASKBLEND_IALPHA,
ebiTFTMBIMaskAlpha = EBI_TFTCTRL_MASKBLEND_IMASKALPHA,
ebiTFTMBEMask = EBI_TFTCTRL_MASKBLEND_EFBMASK,
ebiTFTMBEAlpha = EBI_TFTCTRL_MASKBLEND_EFBALPHA,
ebiTFTMBEMaskAlpha = EBI_TFTCTRL_MASKBLEND_EFBMASKALPHA,
ebiTFTMBEIMask = EBI_TFTCTRL_MASKBLEND_IFBMASK,
ebiTFTMBEIAlpha = EBI_TFTCTRL_MASKBLEND_IFBALPHA,
ebiTFTMBEIMaskAlpha = EBI_TFTCTRL_MASKBLEND_IFBMASKALPHA
}
Control of mask and alpha blending mode.
enum EBI_TFTDDMode_TypeDef {
ebiTFTDDModeDisabled = EBI_TFTCTRL_DD_DISABLED,
ebiTFTDDModeInternal = EBI_TFTCTRL_DD_INTERNAL,
ebiTFTDDModeExternal = EBI_TFTCTRL_DD_EXTERNAL
}
TFT Direct Drive mode.
enum EBI_TFTWidth_TypeDef {
ebiTFTWidthByte = EBI_TFTCTRL_WIDTH_BYTE,
ebiTFTWidthHalfWord = EBI_TFTCTRL_WIDTH_HALFWORD
}
TFT Data Increment Width.

Function Documentation

◆ EBI_Init()

void EBI_Init ( const EBI_Init_TypeDef * ebiInit )

Configure and enable the External Bus Interface.

Parameters
[in] ebiInit The EBI configuration structure.
Note
GPIO lines must be configured as a PUSH_PULL for the correct operation. GPIO and EBI clocks must be enabled in the CMU.

◆ EBI_Disable()

void EBI_Disable ( void )

Disable External Bus Interface.

◆ EBI_BankEnable()

void EBI_BankEnable ( uint32_t banks,
bool enable
)

Enable or disable EBI Bank.

Parameters
[in] banks Banks to reconfigure, mask of EBI_BANK<n> flags.
[in] enable True to enable, false to disable.

◆ EBI_BankAddress()

uint32_t EBI_BankAddress ( uint32_t bank )

Return the base address of the EBI bank.

Parameters
[in] bank A bank to return the start address for.
Returns
an absolute address of the bank.

◆ EBI_NANDFlashEnable()

void EBI_NANDFlashEnable ( uint32_t banks,
bool enable
)

Enable or disable EBI NAND Flash Support.

Parameters
[in] banks Banks to reconfigure, mask of EBI_BANK<n> flags.
[in] enable True to enable, false to disable.

◆ EBI_ChipSelectEnable()

void EBI_ChipSelectEnable ( uint32_t cs,
bool enable
)

Enable or disable EBI Chip Select.

Parameters
[in] cs ChipSelect lines to reconfigure, mask of EBI_CS<n> flags.
[in] enable True to enable, false to disable.

◆ EBI_PolaritySet()

void EBI_PolaritySet ( EBI_Line_TypeDef line,
EBI_Polarity_TypeDef polarity
)

Configure EBI pin polarity.

Parameters
[in] line Which pin/line to configure.
[in] polarity Active high or active low.

◆ EBI_ReadTimingSet()

void EBI_ReadTimingSet ( uint32_t setupCycles,
uint32_t strobeCycles,
uint32_t holdCycles
)

Configure timing values of read bus accesses.

Parameters
[in] setupCycles A number of clock cycles for the address setup before REn is asserted.
[in] strobeCycles The number of cycles the REn is held active. After the specified number of cycles, data is read. If set to 0, 1 cycle is inserted by hardware.
[in] holdCycles The number of cycles CSn is held active after the REn is deasserted.

◆ EBI_WriteTimingSet()

void EBI_WriteTimingSet ( uint32_t setupCycles,
uint32_t strobeCycles,
uint32_t holdCycles
)

Configure timing values of write bus accesses.

Parameters
[in] setupCycles A number of clock cycles for the address setup before WEn is asserted.
[in] strobeCycles A number of cycles WEn is held active. If set to 0, 1 cycle is inserted by hardware.
[in] holdCycles A number of cycles CSn is held active after the WEn is deasserted.

◆ EBI_AddressTimingSet()

void EBI_AddressTimingSet ( uint32_t setupCycles,
uint32_t holdCycles
)

Configure timing values of address latch bus accesses.

Parameters
[in] setupCycles Sets the number of cycles the address is held after ALE is asserted.
[in] holdCycles Sets the number of cycles the address is driven onto the ADDRDAT bus before ALE is asserted. If set 0, 1 cycle is inserted by hardware.

◆ EBI_TFTInit()

void EBI_TFTInit ( const EBI_TFTInit_TypeDef * ebiTFTInit )

Configure and initialize TFT Direct Drive.

Parameters
[in] ebiTFTInit The TFT Initialization structure.

◆ EBI_TFTSizeSet()

void EBI_TFTSizeSet ( uint32_t horizontal,
uint32_t vertical
)

Configure and initialize TFT size settings.

Parameters
[in] horizontal TFT display horizontal size in pixels.
[in] vertical TFT display vertical size in pixels.

◆ EBI_TFTHPorchSet()

void EBI_TFTHPorchSet ( uint32_t front,
uint32_t back,
uint32_t pulseWidth
)

Configure and initialize Horizontal Porch Settings.

Parameters
[in] front Horizontal front porch size in pixels.
[in] back Horizontal back porch size in pixels.
[in] pulseWidth Horizontal synchronization pulse width. Set to required -1.

◆ EBI_TFTVPorchSet()

void EBI_TFTVPorchSet ( uint32_t front,
uint32_t back,
uint32_t pulseWidth
)

Configure Vertical Porch Settings.

Parameters
[in] front Vertical front porch size in pixels.
[in] back Vertical back porch size in pixels.
[in] pulseWidth Vertical synchronization pulse width. Set to required -1.

◆ EBI_TFTTimingSet()

void EBI_TFTTimingSet ( uint32_t dclkPeriod,
uint32_t start,
uint32_t setup,
uint32_t hold
)

Configure TFT Direct Drive Timing Settings.

Parameters
[in] dclkPeriod DCLK period in internal cycles.
[in] start A starting position of the external direct drive, relative to the DCLK inactive edge.
[in] setup A number of cycles that RGB data is driven before the active edge of DCLK.
[in] hold A number of cycles that RGB data is held after the active edge of DCLK.

◆ EBI_BankReadTimingConfig()

void EBI_BankReadTimingConfig ( uint32_t banks,
bool pageMode,
bool prefetch,
bool halfRE
)

Configure read operation parameters for a selected bank.

Parameters
[in] banks A mask of memory bank(s) to configure write timing for.
[in] pageMode Enables or disables the half cycle WE strobe in the last strobe cycle.
[in] prefetch Enables or disables the half cycle WE strobe in the last strobe cycle.
[in] halfRE Enables or disables the half cycle WE strobe in the last strobe cycle.

◆ EBI_BankReadTimingSet()

void EBI_BankReadTimingSet ( uint32_t banks,
uint32_t setupCycles,
uint32_t strobeCycles,
uint32_t holdCycles
)

Configure timing values of read bus accesses.

Parameters
[in] banks A mask of memory bank(s) to configure timing for.
[in] setupCycles A number of clock cycles for address setup before REn is asserted.
[in] strobeCycles The number of cycles the REn is held active. After the specified number of cycles, data is read. If set to 0, 1 cycle is inserted by hardware.
[in] holdCycles The number of cycles CSn is held active after the REn is deasserted.

◆ EBI_BankWriteTimingConfig()

void EBI_BankWriteTimingConfig ( uint32_t banks,
bool writeBufDisable,
bool halfWE
)

Configure write operation parameters for a selected bank.

Parameters
[in] banks A mask of memory bank(s) to configure write timing for.
[in] writeBufDisable If true, disable the write buffer.
[in] halfWE Enables or disables half cycle WE strobe in the last strobe cycle.

◆ EBI_BankWriteTimingSet()

void EBI_BankWriteTimingSet ( uint32_t banks,
uint32_t setupCycles,
uint32_t strobeCycles,
uint32_t holdCycles
)

Configure timing values of write bus accesses.

Parameters
[in] banks A mask of memory bank(s) to configure write timing for.
[in] setupCycles A number of clock cycles for address setup before WEn is asserted.
[in] strobeCycles A number of cycles WEn is held active. If set to 0, 1 cycle is inserted by hardware.
[in] holdCycles Number of cycles CSn is held active after WEn is deasserted.

◆ EBI_BankAddressTimingConfig()

void EBI_BankAddressTimingConfig ( uint32_t banks,
bool halfALE
)

Configure address operation parameters for a selected bank.

Parameters
[in] banks A mask of memory bank(s) to configure write timing for.
[in] halfALE Enables or disables the half cycle ALE strobe in the last strobe cycle.

◆ EBI_BankAddressTimingSet()

void EBI_BankAddressTimingSet ( uint32_t banks,
uint32_t setupCycles,
uint32_t holdCycles
)

Configure timing values of address latch bus accesses.

Parameters
[in] banks A mask of memory bank(s) to configure address timing for.
[in] setupCycles Sets the number of cycles the address is held after ALE is asserted.
[in] holdCycles Sets the number of cycles the address is driven onto the ADDRDAT bus before ALE is asserted. If set 0, 1 cycle is inserted by hardware.

◆ EBI_BankPolaritySet()

void EBI_BankPolaritySet ( uint32_t banks,
EBI_Line_TypeDef line,
EBI_Polarity_TypeDef polarity
)

Configure EBI pin polarity for selected bank(s) for devices with individual timing support.

Parameters
[in] banks A mask of memory bank(s) to configure polarity for.
[in] line Which pin/line to configure.
[in] polarity Active high, or active low.

◆ EBI_BankByteLaneEnable()

void EBI_BankByteLaneEnable ( uint32_t banks,
bool enable
)

Configure Byte Lane Enable for select banks timing support.

Parameters
[in] banks A mask of memory bank(s) to configure polarity for.
[in] enable A flag

◆ EBI_AltMapEnable()

void EBI_AltMapEnable ( bool enable )

Configure the Alternate Address Map support.

Enables or disables 256 MB address range for all banks.

Parameters
[in] enable Set or clear the address map extension.

◆ EBI_TFTEnable()

void EBI_TFTEnable ( EBI_TFTDDMode_TypeDef mode )
inline

Enable or disable TFT Direct Drive.

Parameters
[in] mode Drive from Internal or External memory, or Disable Direct Drive.

◆ EBI_TFTFrameBaseSet()

void EBI_TFTFrameBaseSet ( uint32_t address )
inline

Configure frame buffer pointer.

Parameters
[in] address Frame pointer address, as offset by EBI base address.

◆ EBI_TFTPixelSet()

void EBI_TFTPixelSet ( int pixel,
uint32_t color
)
inline

Set TFT Pixel Color 0 or 1.

Parameters
[in] pixel Which pixel instance to set.
[in] color Color of pixel, 16-bit value.

◆ EBI_TFTDDSet()

void EBI_TFTDDSet ( uint32_t color )
inline

Set TFT Direct Drive Data from Internal Memory.

Parameters
[in] color Color of pixel

◆ EBI_TFTColorFormatSet()

void EBI_TFTColorFormatSet ( EBI_TFTColorFormat_TypeDef color0,
EBI_TFTColorFormat_TypeDef color1
)
inline

Set TFT Color Format.

Parameters
[in] color0 ARGB color format to be used.
[in] color1 RGB color format to be used.

◆ EBI_TFTMaskBlendMode()

void EBI_TFTMaskBlendMode ( EBI_TFTMaskBlend_TypeDef maskBlend )
inline

Masking and Blending Mode Set.

Parameters
[in] maskBlend Masking and alpha blending mode.

◆ EBI_TFTColorSrcSet()

void EBI_TFTColorSrcSet ( EBI_TFTColorSrc_TypeDef colorSrc )
inline

Masking and Blending Color1 Source Set.

Parameters
[in] colorSrc Color1 source.

◆ EBI_TFTAlphaBlendSet()

void EBI_TFTAlphaBlendSet ( uint8_t alpha )
inline

Set TFT Alpha Blending Factor.

Parameters
[in] alpha 8-bit value indicating blending factor.

◆ EBI_TFTMaskSet()

void EBI_TFTMaskSet ( uint32_t mask )
inline

Set TFT mask value.

Data accesses that matches this value are suppressed.

Parameters
[in] mask

◆ EBI_TFTVCount()

uint32_t EBI_TFTVCount ( void )
inline

Get current vertical position counter.

Returns
Returns the current line position for the visible part of a frame.

◆ EBI_TFTHCount()

uint32_t EBI_TFTHCount ( void )
inline

Get current horizontal position counter.

Returns
Returns the current horizontal pixel position within a visible line.

◆ EBI_TFTFBTriggerSet()

void EBI_TFTFBTriggerSet ( EBI_TFTFrameBufTrigger_TypeDef sync )
inline

Set Frame Buffer Trigger.

Frame buffer pointer will be updated either on each horizontal line (hsync) or vertical update (vsync).

Parameters
[in] sync Trigger update of frame buffer pointer on vertical or horizontal sync.

◆ EBI_TFTHStrideSet()

void EBI_TFTHStrideSet ( uint32_t nbytes )
inline

Set horizontal TFT stride value in number of bytes.

Parameters
[in] nbytes Number of bytes to add to frame buffer pointer after each horizontal line update.

◆ EBI_IntClear()

void EBI_IntClear ( uint32_t flags )
inline

Clear one or more pending EBI interrupts.

Parameters
[in] flags Pending EBI interrupt source to clear. Use a logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn).

◆ EBI_IntSet()

void EBI_IntSet ( uint32_t flags )
inline

Set one or more pending EBI interrupts.

Parameters
[in] flags EBI interrupt sources to set to pending. Use a logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn).

◆ EBI_IntDisable()

void EBI_IntDisable ( uint32_t flags )
inline

Disable one or more EBI interrupts.

Parameters
[in] flags EBI interrupt sources to disable. Use logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn)

◆ EBI_IntEnable()

void EBI_IntEnable ( uint32_t flags )
inline

Enable one or more EBI interrupts.

Parameters
[in] flags EBI interrupt sources to enable. Use logical OR combination of valid interrupt flags for the EBI module (EBI_IF_nnn)

◆ EBI_IntGet()

uint32_t EBI_IntGet ( void )
inline

Get pending EBI interrupt flags.

Note
Event bits are not cleared by the use of this function.
Returns
EBI interrupt sources pending, a logical combination of valid EBI interrupt flags, EBI_IF_nnn.

◆ EBI_IntGetEnabled()

uint32_t EBI_IntGetEnabled ( void )
inline

Get enabled and pending EBI interrupt flags.

Useful for handling more interrupt sources in the same interrupt handler.

Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled EBI interrupt sources. The return value is the bitwise AND of
  • the enabled interrupt sources in EBI_IEN and
  • the pending interrupt flags EBI_IF.

◆ EBI_StartNandEccGen()

void EBI_StartNandEccGen ( void )
inline

Start ECC generator on NAND flash transfers.

◆ EBI_StopNandEccGen()

uint32_t EBI_StopNandEccGen ( void )
inline

Stop NAND flash ECC generator and return generated ECC.

Returns
The generated ECC.

Macro Definition Documentation

◆ EBI_BANK0

#define EBI_BANK0   (uint32_t)(1 << 1)

EBI address bank 0.

*
* ---------               ---------
* |       |  /|       |\  | Ext.  |
* |  EBI  | / --------- \ | Async |
* |       | \ --------- / | Device|
* |       |  \|       |/  |       |
* ---------               ---------
*         Parallel interface
*
* 

◆ EBI_BANK1

#define EBI_BANK1   (uint32_t)(1 << 2)

EBI address bank 1.

◆ EBI_BANK2

#define EBI_BANK2   (uint32_t)(1 << 3)

EBI address bank 2.

◆ EBI_BANK3

#define EBI_BANK3   (uint32_t)(1 << 4)

EBI address bank 3.

◆ EBI_CS0

#define EBI_CS0   (uint32_t)(1 << 1)

EBI chip select line 0.

◆ EBI_CS1

#define EBI_CS1   (uint32_t)(1 << 2)

EBI chip select line 1.

◆ EBI_CS2

#define EBI_CS2   (uint32_t)(1 << 3)

EBI chip select line 2.

◆ EBI_CS3

#define EBI_CS3   (uint32_t)(1 << 4)

EBI chip select line 3.

◆ EBI_GENERIC_ALB_A0

#define EBI_GENERIC_ALB_A0   EBI_ROUTEPEN_ALB_A0

Pin Enable Lower Bound EBI_A[0] and upwards.

◆ EBI_GENERIC_ALB_A8

#define EBI_GENERIC_ALB_A8   EBI_ROUTEPEN_ALB_A8

Pin Enable Lower Bound EBI_A[8] and upwards.

◆ EBI_GENERIC_ALB_A16

#define EBI_GENERIC_ALB_A16   EBI_ROUTEPEN_ALB_A16

Pin Enable Lower Bound EBI_A[16] and upwards.

◆ EBI_GENERIC_ALB_A24

#define EBI_GENERIC_ALB_A24   EBI_ROUTEPEN_ALB_A24

Pin Enable Lower Bound EBI_A[24] and upwards.

◆ EBI_GENERIC_APEN_A0

#define EBI_GENERIC_APEN_A0   EBI_ROUTEPEN_APEN_A0

All EBI_A pins enabled.

◆ EBI_GENERIC_APEN_A5

#define EBI_GENERIC_APEN_A5   EBI_ROUTEPEN_APEN_A5

EBI_A[4:L] pins enabled.

◆ EBI_GENERIC_APEN_A6

#define EBI_GENERIC_APEN_A6   EBI_ROUTEPEN_APEN_A6

EBI_A[5:L] pins enabled.

◆ EBI_GENERIC_APEN_A7

#define EBI_GENERIC_APEN_A7   EBI_ROUTEPEN_APEN_A7

EBI_A[6:L] pins enabled.

◆ EBI_GENERIC_APEN_A8

#define EBI_GENERIC_APEN_A8   EBI_ROUTEPEN_APEN_A8

EBI_A[7:L] pins enabled.

◆ EBI_GENERIC_APEN_A9

#define EBI_GENERIC_APEN_A9   EBI_ROUTEPEN_APEN_A9

EBI_A[8:L] pins enabled.

◆ EBI_GENERIC_APEN_A10

#define EBI_GENERIC_APEN_A10   EBI_ROUTEPEN_APEN_A10

EBI_A[9:L] pins enabled.

◆ EBI_GENERIC_APEN_A11

#define EBI_GENERIC_APEN_A11   EBI_ROUTEPEN_APEN_A11

EBI_A[10:L] pins enabled.

◆ EBI_GENERIC_APEN_A12

#define EBI_GENERIC_APEN_A12   EBI_ROUTEPEN_APEN_A12

EBI_A[11:L] pins enabled.

◆ EBI_GENERIC_APEN_A13

#define EBI_GENERIC_APEN_A13   EBI_ROUTEPEN_APEN_A13

EBI_A[12:L] pins enabled.

◆ EBI_GENERIC_APEN_A14

#define EBI_GENERIC_APEN_A14   EBI_ROUTEPEN_APEN_A14

EBI_A[13:L] pins enabled.

◆ EBI_GENERIC_APEN_A15

#define EBI_GENERIC_APEN_A15   EBI_ROUTEPEN_APEN_A15

EBI_A[14:L] pins enabled.

◆ EBI_GENERIC_APEN_A16

#define EBI_GENERIC_APEN_A16   EBI_ROUTEPEN_APEN_A16

EBI_A[15:L] pins enabled.

◆ EBI_GENERIC_APEN_A17

#define EBI_GENERIC_APEN_A17   EBI_ROUTEPEN_APEN_A17

EBI_A[16:L] pins enabled.

◆ EBI_GENERIC_APEN_A18

#define EBI_GENERIC_APEN_A18   EBI_ROUTEPEN_APEN_A18

EBI_A[17:L] pins enabled.

◆ EBI_GENERIC_APEN_A19

#define EBI_GENERIC_APEN_A19   EBI_ROUTEPEN_APEN_A19

EBI_A[18:L] pins enabled.

◆ EBI_GENERIC_APEN_A20

#define EBI_GENERIC_APEN_A20   EBI_ROUTEPEN_APEN_A20

EBI_A[19:L] pins enabled.

◆ EBI_GENERIC_APEN_A21

#define EBI_GENERIC_APEN_A21   EBI_ROUTEPEN_APEN_A21

EBI_A[20:L] pins enabled.

◆ EBI_GENERIC_APEN_A22

#define EBI_GENERIC_APEN_A22   EBI_ROUTEPEN_APEN_A22

EBI_A[21:L] pins enabled.

◆ EBI_GENERIC_APEN_A23

#define EBI_GENERIC_APEN_A23   EBI_ROUTEPEN_APEN_A23

EBI_A[22:L] pins enabled.

◆ EBI_GENERIC_APEN_A24

#define EBI_GENERIC_APEN_A24   EBI_ROUTEPEN_APEN_A24

EBI_A[23:L] pins enabled.

◆ EBI_GENERIC_APEN_A25

#define EBI_GENERIC_APEN_A25   EBI_ROUTEPEN_APEN_A25

EBI_A[24:L] pins enabled.

◆ EBI_GENERIC_APEN_A26

#define EBI_GENERIC_APEN_A26   EBI_ROUTEPEN_APEN_A26

EBI_A[25:L] pins enabled.

◆ EBI_GENERIC_APEN_A27

#define EBI_GENERIC_APEN_A27   EBI_ROUTEPEN_APEN_A27

EBI_A[26:L] pins enabled.

◆ EBI_GENERIC_APEN_A28

#define EBI_GENERIC_APEN_A28   EBI_ROUTEPEN_APEN_A28

EBI_A[27:L] pins enabled.

◆ EBI_INIT_DEFAULT

#define EBI_INIT_DEFAULT

Default configuration for EBI initialization structures.

◆ EBI_TFTINIT_DEFAULT

#define EBI_TFTINIT_DEFAULT
Value:
{ \
ebiTFTBank0, /* Select EBI Bank 0. */ \
ebiTFTWidthHalfWord, /* Select 2-byte increments. */ \
ebiTFTColorSrcMem, /* Use memory as source for mask/blending. */ \
ebiTFTInterleaveUnlimited, /* Unlimited interleaved accesses. */ \
ebiTFTFrameBufTriggerVSync, /* VSYNC as frame buffer update trigger. */ \
false, /* Drive DCLK from negative edge of internal clock. */ \
ebiTFTMBDisabled, /* No masking and alpha blending enabled. */ \
ebiTFTDDModeExternal, /* Drive from external memory. */ \
ebiActiveLow, /* CS Active Low polarity. */ \
ebiActiveLow, /* DCLK Active Low polarity. */ \
ebiActiveLow, /* DATAEN Active Low polarity. */ \
ebiActiveLow, /* HSYNC Active Low polarity. */ \
ebiActiveLow, /* VSYNC Active Low polarity. */ \
320, /* Horizontal size in pixels. */ \
1, /* Horizontal Front Porch. */ \
29, /* Horizontal Back Porch. */ \
2, /* Horizontal Synchronization Pulse Width. */ \
240, /* Vertical size in pixels. */ \
1, /* Vertical Front Porch. */ \
4, /* Vertical Back Porch. */ \
2, /* Vertical Synchronization Pulse Width. */ \
0x0000, /* Address offset to EBI memory base. */ \
5, /* DCLK Period. */ \
2, /* DCLK Start. */ \
1, /* DCLK Setup cycles. */ \
1, /* DCLK Hold cycles. */ \
}

Default configuration for EBI TFT initialization structure.

Enumeration Type Documentation

◆ EBI_Mode_TypeDef

EBI Mode of operation.

Enumerator
ebiModeD8A8

8 data bits, 8 address bits.

ebiModeD16A16ALE

16 data bits, 16 address bits, using address latch enable.

ebiModeD8A24ALE

8 data bits, 24 address bits, using address latch enable.

ebiModeD16

Mode D16.

◆ EBI_Polarity_TypeDef

EBI Polarity configuration.

Enumerator
ebiActiveLow

Active Low.

ebiActiveHigh

Active High.

◆ EBI_Line_TypeDef

EBI Pin Line types.

Enumerator
ebiLineARDY

Address Ready line.

ebiLineALE

Address Latch Enable line.

ebiLineWE

Write Enable line.

ebiLineRE

Read Enable line.

ebiLineCS

Chip Select line.

ebiLineBL

BL line.

ebiLineTFTVSync

TFT VSYNC line.

ebiLineTFTHSync

TFT HSYNC line.

ebiLineTFTDataEn

TFT Data enable line.

ebiLineTFTDClk

TFT DCLK line.

ebiLineTFTCS

TFT Chip select line.

◆ EBI_ALow_TypeDef

Address Pin Enable, lower limit - lower range of pins to enable.

Enumerator
ebiALowA0

Address lines EBI_A[0] and upwards are enabled by APEN.

ebiALowA8

Address lines EBI_A[8] and upwards are enabled by APEN.

ebiALowA16

Address lines EBI_A[16] and upwards are enabled by APEN.

ebiALowA24

Address lines EBI_A[24] and upwards are enabled by APEN.

◆ EBI_AHigh_TypeDef

Address Pin Enable, high limit - higher limit of pins to enable.

Enumerator
ebiAHighA0

All EBI_A pins are disabled.

ebiAHighA5

All EBI_A[4:ALow] are enabled.

ebiAHighA6

All EBI_A[5:ALow] are enabled.

ebiAHighA7

All EBI_A[6:ALow] are enabled.

ebiAHighA8

All EBI_A[7:ALow] are enabled.

ebiAHighA9

All EBI_A[8:ALow] are enabled.

ebiAHighA10

All EBI_A[9:ALow] are enabled.

ebiAHighA11

All EBI_A[10:ALow] are enabled.

ebiAHighA12

All EBI_A[11:ALow] are enabled.

ebiAHighA13

All EBI_A[12:ALow] are enabled.

ebiAHighA14

All EBI_A[13:ALow] are enabled.

ebiAHighA15

All EBI_A[14:ALow] are enabled.

ebiAHighA16

All EBI_A[15:ALow] are enabled.

ebiAHighA17

All EBI_A[16:ALow] are enabled.

ebiAHighA18

All EBI_A[17:ALow] are enabled.

ebiAHighA19

All EBI_A[18:ALow] are enabled.

ebiAHighA20

All EBI_A[19:ALow] are enabled.

ebiAHighA21

All EBI_A[20:ALow] are enabled.

ebiAHighA22

All EBI_A[21:ALow] are enabled.

ebiAHighA23

All EBI_A[22:ALow] are enabled.

ebiAHighA24

All EBI_A[23:ALow] are enabled.

ebiAHighA25

All EBI_A[24:ALow] are enabled.

ebiAHighA26

All EBI_A[25:ALow] are enabled.

ebiAHighA27

All EBI_A[26:ALow] are enabled.

ebiAHighA28

All EBI_A[27:ALow] are enabled.

◆ EBI_TFTBank_TypeDef

EBI TFT Graphics Bank Select.

Enumerator
ebiTFTBank0

Memory BANK0 contains frame buffer.

ebiTFTBank1

Memory BANK1 contains frame buffer.

ebiTFTBank2

Memory BANK2 contains frame buffer.

ebiTFTBank3

Memory BANK3 contains frame buffer.

◆ EBI_TFTColorFormat_TypeDef

EBI TFT Color format.

Enumerator
ebiTFTARGB0555

Set ARGB (Alpha, Red, Green, Blue) color format to 0555.

ebiTFTARGB0565

Set ARGB (Alpha, Red, Green, Blue) color format to 0565.

ebiTFTARGB0666

Set ARGB (Alpha, Red, Green, Blue) color format to 0666.

ebiTFTARGB0888

Set ARGB (Alpha, Red, Green, Blue) color format to 0888.

ebiTFTARGB5555

Set ARGB (Alpha, Red, Green, Blue) color format to 5555.

ebiTFTARGB6565

Set ARGB (Alpha, Red, Green, Blue) color format to 6565.

ebiTFTARGB6666

Set ARGB (Alpha, Red, Green, Blue) color format to 6666.

ebiTFTARGB8888

Set ARGB (Alpha, Red, Green, Blue) color format to 8888.

ebiTFTRGB555

Set RGB (Red, Green, Blue) color format to 555.

ebiTFTRGB565

Set RGB (Red, Green, Blue) color format to 565.

ebiTFTRGB666

Set RGB (Red, Green, Blue) color format to 666.

ebiTFTRGB888

Set RGB (Red, Green, Blue) color format to 888.

◆ EBI_TFTColorSrc_TypeDef

Masking and Alpha blending source color.

Enumerator
ebiTFTColorSrcMem

Use memory as source color for masking/alpha blending.

ebiTFTColorSrcPixel1

Use PIXEL1 register as source color for masking/alpha blending.

◆ EBI_TFTInterleave_TypeDef

Bus Data Interleave Mode.

Enumerator
ebiTFTInterleaveUnlimited

Unlimited interleaved accesses per EBI_DCLK period.

Can cause jitter.

ebiTFTInterleaveOnePerDClk

Allow 1 interleaved access per EBI_DCLK period.

ebiTFTInterleavePorch

Only allow accesses during porch periods.

◆ EBI_TFTFrameBufTrigger_TypeDef

Control frame base pointer copy.

Enumerator
ebiTFTFrameBufTriggerVSync

Trigger update of frame buffer pointer on vertical sync.

ebiTFTFrameBufTriggerHSync

Trigger update of frame buffer pointer on horizontal sync.

◆ EBI_TFTMaskBlend_TypeDef

Control of mask and alpha blending mode.

Enumerator
ebiTFTMBDisabled

Masking and blending are disabled.

ebiTFTMBIMask

Internal masking.

ebiTFTMBIAlpha

Internal alpha blending.

ebiTFTMBIMaskAlpha

Internal masking and alpha blending are enabled.

ebiTFTMBEMask

External masking.

ebiTFTMBEAlpha

External alpha blending.

ebiTFTMBEMaskAlpha

External masking and alpha blending.

ebiTFTMBEIMask

Internal Frame Buffer masking.

ebiTFTMBEIAlpha

Internal Frame Buffer alpha blending.

ebiTFTMBEIMaskAlpha

Internal Frame Buffer masking and alpha blending.

◆ EBI_TFTDDMode_TypeDef

TFT Direct Drive mode.

Enumerator
ebiTFTDDModeDisabled

Disabled.

ebiTFTDDModeInternal

Direct Drive from internal memory.

ebiTFTDDModeExternal

Direct Drive from external memory.

◆ EBI_TFTWidth_TypeDef

TFT Data Increment Width.

Enumerator
ebiTFTWidthByte

Pixel increments are 1 byte at a time.

ebiTFTWidthHalfWord

Pixel increments are 2 bytes (half word).