QSPI_StigCmd_TypeDef Struct Reference

Defines command to be executed using STIG mechanism.

#include <em_qspi.h>

Data Fields

uint8_t cmdOpcode
Command op-code.
uint16_t readDataSize
Number of Read Data Bytes.
uint8_t addrSize
Number of Address Bytes.
uint8_t writeDataSize
Number of Write Data Bytes.
uint8_t dummyCycles
Number of dummy cycles.
bool modeBitEnable
Mode Bit Configuration register are sent following the address bytes.
uint32_t address
Flash command address.
void * readBuffer
Buffer for read data.
void * writeBuffer
Buffer with data to write.

Defines command to be executed using STIG mechanism.

Field Documentation

◆ cmdOpcode

uint8_t QSPI_StigCmd_TypeDef::cmdOpcode

Command op-code.

◆ readDataSize

uint16_t QSPI_StigCmd_TypeDef::readDataSize

Number of Read Data Bytes.

◆ addrSize

uint8_t QSPI_StigCmd_TypeDef::addrSize

Number of Address Bytes.

◆ writeDataSize

uint8_t QSPI_StigCmd_TypeDef::writeDataSize

Number of Write Data Bytes.

◆ dummyCycles

uint8_t QSPI_StigCmd_TypeDef::dummyCycles

Number of dummy cycles.

◆ modeBitEnable

bool QSPI_StigCmd_TypeDef::modeBitEnable

Mode Bit Configuration register are sent following the address bytes.

◆ address

uint32_t QSPI_StigCmd_TypeDef::address

Flash command address.

◆ readBuffer

void* QSPI_StigCmd_TypeDef::readBuffer

Buffer for read data.

◆ writeBuffer

void* QSPI_StigCmd_TypeDef::writeBuffer

Buffer with data to write.