EMU_DCDCInit_TypeDef Struct Reference
DCDC initialization structure.
#include <em_emu.h>
Data Fields |
|
EMU_PowerConfig_TypeDef | powerConfig |
Device external power configuration.
|
|
EMU_DcdcMode_TypeDef | dcdcMode |
DCDC regulator operating mode in EM0/1.
|
|
uint16_t | mVout |
Target output voltage (mV).
|
|
uint16_t | em01LoadCurrent_mA |
Estimated average load current in EM0/1.
|
|
uint16_t | em234LoadCurrent_uA |
Estimated average load current in EM2 (uA).
|
|
uint16_t | maxCurrent_mA |
Maximum average DCDC output current (mA).
|
|
EMU_DcdcAnaPeripheralPower_TypeDef | anaPeripheralPower |
Select analog peripheral power in DCDC-to-DVDD mode.
|
|
EMU_DcdcLnReverseCurrentControl_TypeDef | reverseCurrentControl |
Low-noise reverse current control.
|
|
EMU_DcdcLnCompCtrl_TypeDef | dcdcLnCompCtrl |
DCDC Low-noise mode compensator control.
|
|
DCDC initialization structure.
Field Documentation
◆ powerConfig
EMU_PowerConfig_TypeDef EMU_DCDCInit_TypeDef::powerConfig |
Device external power configuration.
emuPowerConfig_DcdcToDvdd is currently the only supported mode.
◆ dcdcMode
EMU_DcdcMode_TypeDef EMU_DCDCInit_TypeDef::dcdcMode |
DCDC regulator operating mode in EM0/1.
◆ mVout
uint16_t EMU_DCDCInit_TypeDef::mVout |
Target output voltage (mV).
◆ em01LoadCurrent_mA
uint16_t EMU_DCDCInit_TypeDef::em01LoadCurrent_mA |
Estimated average load current in EM0/1.
(mA). This estimate is also used for EM1 optimization; if EM1 current is expected to be higher than EM0, then this parameter should hold the higher EM1 current.
◆ em234LoadCurrent_uA
uint16_t EMU_DCDCInit_TypeDef::em234LoadCurrent_uA |
Estimated average load current in EM2 (uA).
This estimate is also used for EM3 and 4 optimization; if EM3 or 4 current is expected to be higher than EM2, then this parameter should hold the higher EM3 or 4 current.
◆ maxCurrent_mA
uint16_t EMU_DCDCInit_TypeDef::maxCurrent_mA |
Maximum average DCDC output current (mA).
This can be set to the maximum for the power source, for example the maximum for a battery.
◆ anaPeripheralPower
EMU_DcdcAnaPeripheralPower_TypeDef EMU_DCDCInit_TypeDef::anaPeripheralPower |
Select analog peripheral power in DCDC-to-DVDD mode.
◆ reverseCurrentControl
EMU_DcdcLnReverseCurrentControl_TypeDef EMU_DCDCInit_TypeDef::reverseCurrentControl |
Low-noise reverse current control.
NOTE: this parameter uses special encoding: >= 0 is forced CCM mode where the parameter is used as the reverse current threshold in mA. -1 is encoded as emuDcdcLnHighEfficiencyMode (EFM32 only).
◆ dcdcLnCompCtrl
EMU_DcdcLnCompCtrl_TypeDef EMU_DCDCInit_TypeDef::dcdcLnCompCtrl |
DCDC Low-noise mode compensator control.