ACMP_VBConfig_TypeDef Struct Reference

VB Configuration structure.

#include <em_acmp.h>

Data Fields

ACMP_VBInput_TypeDef input
VB Voltage input source.
uint32_t div0
A divider for VB voltage input source when ACMP output is 0.
uint32_t div1
A divider for VB voltage input source when ACMP output is 1.

VB Configuration structure.

This structure is used to configure the VB voltage input source and its dividers.

Field Documentation

◆ input

ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input

VB Voltage input source.

◆ div0

uint32_t ACMP_VBConfig_TypeDef::div0

A divider for VB voltage input source when ACMP output is 0.

This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div0 + 1) / 64

◆ div1

uint32_t ACMP_VBConfig_TypeDef::div1

A divider for VB voltage input source when ACMP output is 1.

This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.

VB divided = VB input * (div1 + 1) / 64