BootloadBootloader Core
Description
Methods to verify and bootload application images.
Functions |
|
| bool | bootload_verifyApplication (uint32_t startAddress) |
| void | bootload_bootloaderCallback (uint32_t offset, uint8_t data[], size_t length, void *context) |
| void | bootload_applicationCallback (uint32_t address, uint8_t data[], size_t length, void *context) |
| bool | bootloader_enforceSecureBoot (void) |
| bool | bootload_commitBootloaderUpgrade (uint32_t upgradeAddress, uint32_t size) |
| bool | bootload_checkSeUpgradeVersion (uint32_t upgradeVersion) |
| bool | bootload_commitSeUpgrade (uint32_t upgradeAddress) |
Function Documentation
| bool bootload_verifyApplication | ( | uint32_t |
startAddress
|
) |
Verify the application image stored in the Flash memory starting at the address startAddress.
If secure boot is enforced, the function will only return true if the cryptographic signature of the application is valid. Else, the application is verified according to the signature type defined in the ApplicationProperties_t structure embedded in the application. Silicon Labs wireless stacks declare this structure. Applications, which are not using a full wireless stack may need to instantiate the structure.
Examples of results when secure boot is not enforced:
- App has no signature: Valid if initial stack pointer and program counter have reasonable values
- App has CRC checksum: Valid if checksum is valid
- App has ECDSA signature: Valid if ECDSA signature is valid.
When secure boot is enforced, only ECDSA-signed applications with a valid signature are considered valid.
- Parameters
-
[in] startAddressStarting address of the application
- Returns
- True if the image is deemed valid
| void bootload_bootloaderCallback | ( | uint32_t |
offset,
|
| uint8_t |
data[],
|
||
| size_t |
length,
|
||
| void * |
context
|
||
| ) |
Bootloader upgrade callback implementation.
- Parameters
-
offsetOffset of bootloader data (byte counter incrementing from 0) dataRaw bootloader data lengthSize in bytes of raw bootloader data. contextA context variable defined by the implementation that is implementing this callback.
| void bootload_applicationCallback | ( | uint32_t |
address,
|
| uint8_t |
data[],
|
||
| size_t |
length,
|
||
| void * |
context
|
||
| ) |
Image data callback implementation.
- Parameters
-
addressAddress (inside the raw image) the data starts at dataRaw image data lengthSize in bytes of raw image data. Always constrained to a multiple of four. contextA context variable defined by the implementation that is implementing this callback.
| bool bootloader_enforceSecureBoot | ( | void |
|
) |
Indicates whether the bootloader should enforce a secure boot.
- Returns
- True if secure boot is to be enforced.
| bool bootload_commitBootloaderUpgrade | ( | uint32_t |
upgradeAddress,
|
| uint32_t |
size
|
||
| ) |
Perform a bootloader upgrade using the upgrade image present at upgradeAddress with length size.
If the bootloader upgrade process starts successfully, this function does not return and execution will resume from the reset handler of the upgraded bootloader.
- Parameters
-
[in] upgradeAddressThe starting address of the upgrade image [in] sizeThe length of the upgrade image in bytes
- Returns
- False if the bootloader upgrade process didn't start
| bool bootload_checkSeUpgradeVersion | ( | uint32_t |
upgradeVersion
|
) |
Check that an SE upgrade with a given version number is allowed to be installed.
This will only be true if the upgrade version is higher than the running version.
- Parameters
-
[in] upgradeVersionThe version of the SE upgrade image
- Returns
- True if the SE upgrade image should be installed
| bool bootload_commitSeUpgrade | ( | uint32_t |
upgradeAddress
|
) |
Perform an SE upgrade using the upgrade image present at upgradeAddress.
If the SE upgrade process starts successfully, this function does not return and execution will resume from the reset handler after the SE upgrade is complete.
- Parameters
-
[in] upgradeAddressThe starting address of the upgrade image.
- Returns
- False if the SE upgrade process didn't start.