Bootload InfoPlugin > Storage
Description
Indicates which firmware update image should be bootloaded next.
This plugin provides the bootloader with support for storing multiple images and attempting to bootload a prioritized list. The Bootload Information struct is placed at a known location in storage, and points to a list of images to attempt to bootload.
While the Bootload Information list of images to attempt to bootload has a compile-time configurable size, the bootloader is capable of handling lists of images with different sizes, e.g., if a bootloader upgrade changes the slot layout or if a storage device that was initialized on a different device is used.
If only one storage slot is available, the functions available in this API will do nothing and return applicable error codes ( BOOTLOADER_OK for storage_getBootloadList and storage_setBootloadList , and BOOTLOADER_ERROR_BOOTLOAD_LIST_FULL for storage_appendBootloadList ).
Data Structures |
|
| struct | BootloadInfo_t |
Macros |
|
| #define | BTL_STORAGE_BOOTLOADINFO_MAGIC 0xE18F5239UL |
|
Magic word indicating
BootloadInfo_t
struct.
|
|
| #define | BTL_STORAGE_BOOTLOADINFO_VERSION 0x00000001UL |
|
Version number for the
BootloadInfo_t
struct.
|
|
| #define | BTL_STORAGE_BOOTLOAD_LIST_MAX_LENGTH 16UL |
|
Maximum number of items in the
BootloadInfo_t::bootloadList
.
|
|
Functions |
|
| int32_t | storage_getBootloadList (int32_t slotIds[], size_t length) |
| int32_t | storage_setBootloadList (int32_t slotIds[], size_t length) |
| int32_t | storage_appendBootloadList (int32_t slotId) |
Function Documentation
| int32_t storage_getBootloadList | ( | int32_t |
slotIds[],
|
| size_t |
length
|
||
| ) |
Get list of firmware update images to attempt to bootload.
- Parameters
-
[out] slotIdsPointer to array of integers to fill with slot IDs, or -1 if list position does not contain a valid slot ID [in] lengthNumber of slot IDs to get
- Returns
- Error code: BOOTLOADER_OK if list of slots was successfully filled else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_setBootloadList | ( | int32_t |
slotIds[],
|
| size_t |
length
|
||
| ) |
Set list of firmware update images to attempt to bootload.
- Parameters
-
[in] slotIdsPointer to array of slot IDs to set [in] lengthNumber of slot IDs to set
- Returns
- Error code: BOOTLOADER_OK if list of slots was successfully filled
| int32_t storage_appendBootloadList | ( | int32_t |
slotId
|
) |
Append a storage slot to the list of storage slots to try bootloading from.
- Parameters
-
[in] slotIdID of the slot
- Returns
- Error code: BOOTLOADER_OK if slot was successfully appended