DebugPlugin
Description
Debug Plugin.
This plugin provides the bootloader with support for debugging functions. The plugin implements two types of debugging functionality:
- Defining BTL_PLUGIN_DEBUG_ASSERT enables assertions on compile-time configurable parameters in the bootloader
- Defining BTL_PLUGIN_DEBUG_PRINT enables debug prints at strategic points in the code.
Macros |
|
| #define | BTL_ASSERT (exp) ((void)(exp)) |
|
Assertion in bootloader.
|
|
| #define | BTL_DEBUG_INIT () do {} while (0) |
|
Initialize debug output.
|
|
| #define | BTL_DEBUG_PRINT (str) do {} while (0) |
|
Print a string to debug out.
|
|
| #define | BTL_DEBUG_PRINTLN (str) do {} while (0) |
|
Print a string followed by a newline to debug out.
|
|
| #define | BTL_DEBUG_PRINTC (chr) do {} while (0) |
|
Print a character to debut out.
|
|
| #define | BTL_DEBUG_PRINT_CHAR_HEX (number) do {} while (0) |
|
Print a single hex byte.
|
|
| #define | BTL_DEBUG_PRINT_SHORT_HEX (number) do {} while (0) |
|
Print two hex bytes.
|
|
| #define | BTL_DEBUG_PRINT_WORD_HEX (number) do {} while (0) |
|
Print a hex word.
|
|
| #define | BTL_DEBUG_PRINT_LF () do {} while (0) |
|
Print a newline.
|
|