BootloaderStorageFunctions Struct ReferenceApplication Interface > Application Storage Interface
Description
Storage API accessible from the application.
Definition at line
101
of file
btl_interface_storage.h
.
#include <
btl_interface_storage.h
>
Data Fields |
|
| uint32_t | version |
|
Version of this struct.
|
|
| void(* | getInfo )( BootloaderStorageInformation_t *info) |
|
Get information about the storage – capabilities, layout, configuration.
|
|
| int32_t(* | getSlotInfo )(uint32_t slotId, BootloaderStorageSlot_t *slot) |
|
Get information about storage slot – size, location.
|
|
| int32_t(* | read )(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length) |
|
Read bytes from slot into buffer.
|
|
| int32_t(* | write )(uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t length) |
|
Write bytes from buffer into slot.
|
|
| int32_t(* | erase )(uint32_t slotId) |
|
Erase an entire slot.
|
|
| int32_t(* | setImagesToBootload )(int32_t *slotIds, size_t length) |
|
Mark a list of slots for bootload.
|
|
| int32_t(* | getImagesToBootload )(int32_t *slotIds, size_t length) |
|
Mark a list of slots for bootload.
|
|
| int32_t(* | appendImageToBootloadList )(int32_t slotId) |
|
Append a slot to bootload list.
|
|
| int32_t(* | initParseImage )(uint32_t slotId, BootloaderParserContext_t *context, size_t contextSize) |
|
Start image parsing.
|
|
| int32_t(* | verifyImage )( BootloaderParserContext_t *context, BootloaderParserCallback_t metadataCallback) |
|
Continue image verification.
|
|
| int32_t(* | getImageInfo )( BootloaderParserContext_t *context, ApplicationData_t *appInfo, uint32_t *bootloaderVersion) |
|
Get app and bootloader upgrade information from storage slot.
|
|
| bool(* | isBusy )(void) |
|
Check whether the bootloader storage is busy.
|
|
| int32_t(* | readRaw )(uint32_t address, uint8_t *buffer, size_t length) |
|
Read raw bytes from storage.
|
|
| int32_t(* | writeRaw )(uint32_t address, uint8_t *buffer, size_t length) |
|
Write bytes to raw storage.
|
|
| int32_t(* | eraseRaw )(uint32_t address, size_t length) |
|
Erase storage.
|
|
The documentation for this struct was generated from the following file:
-
btl_interface_storage.h