StoragePlugin
Description
Storage plugin.
This plugin provides the bootloader with multiple storage options. All storage implementations have to provide a slot-based API to access image files to be bootloaded.
Some storage implementations also support a raw storage API to access the underlying storage medium. This can be used by applications to store other data in parts of the storage medium that are not used for bootloading.
Storage Implementations
Internal Flash
SPI Flash
- Spansion S25FL208K (8Mbit)
- Winbond W25X20BV (2Mbit), W25Q80BV (8Mbit)
- Macronix MX25L2006E (2Mbit), MX25L4006E (4Mbit), MX25L8006E (8Mbit), MX25R8035F (8Mbit low power), MX25L1606E (16Mbit), MX25U1635E (16Mbit 2Volt), MX25R6435F (64Mbit low power)
- Atmel/Adesto AT25DF041A (4Mbit), AT25DF081A (8Mbit)
- Numonyx/Micron M25P20 (2Mbit), M25P40 (4Mbit), M25P80 (8Mbit), M25P16 (16Mbit)
- ISSI IS25LQ025B (256Kbit), IS25LQ512B (512Kbit), IS25LQ010B (1Mbit), IS25LQ020B (2Mbit), IS25LQ040B (4Mbit)
Modules |
|
| Bootload Info | |
|
Indicates which firmware update image should be bootloaded next.
|
|
| SPI Flash Configurations | |
|
Configuration parameters for SPI flashes.
|
|
Data Structures |
|
| struct | BootloaderStorageLayout_t |
|
Information about the storage backend.
|
|
Macros |
|
| #define | BOOTLOADER_STORAGE_FUNCTIONS_VERSION 0x00000100 |
|
Version number for bootloader storage functions struct.
|
|
Functions |
|
| int32_t | storage_init (void) |
| int32_t | storage_main (void) |
| int32_t | storage_shutdown (void) |
| void | storage_getInfo ( BootloaderStorageInformation_t *info) |
| int32_t | storage_getSlotInfo (uint32_t slotId, BootloaderStorageSlot_t *slot) |
| int32_t | storage_getSlotMetadata ( BootloaderParserContext_t *context, ApplicationData_t *appInfo, uint32_t *bootloaderVersion) |
| int32_t | storage_initParseSlot (uint32_t slotId, BootloaderParserContext_t *context, size_t contextSize) |
| int32_t | storage_verifySlot ( BootloaderParserContext_t *context, BootloaderParserCallback_t metadataCallback) |
| bool | storage_upgradeSeFromSlot (uint32_t slotId) |
| bool | storage_bootloadBootloaderFromSlot (uint32_t slotId, uint32_t version) |
| bool | storage_bootloadApplicationFromSlot (uint32_t slotId, uint32_t version) |
| int32_t | storage_eraseSlot (uint32_t slotId) |
| int32_t | storage_readSlot (uint32_t slotId, uint32_t offset, uint8_t *buffer, size_t numBytes) |
| int32_t | storage_writeSlot (uint32_t slotId, uint32_t offset, uint8_t *data, size_t numBytes) |
| int32_t | storage_readRaw (uint32_t address, uint8_t *buffer, size_t numBytes) |
| int32_t | storage_writeRaw (uint32_t address, uint8_t *data, size_t numBytes) |
| int32_t | storage_eraseRaw (uint32_t address, size_t length) |
| bool | storage_isBusy (void) |
Function Documentation
| int32_t storage_init | ( | void |
|
) |
Initialize the storage plugin.
- Returns
- Error code indicating success or failure.
- Return values
-
BOOTLOADER_OKon success BOOTLOADER_ERROR_INIT_STORAGEon failure
| int32_t storage_main | ( | void |
|
) |
Main function for storage plugin.
- Returns
- BOOTLOADER_OK on success, else error code
| int32_t storage_shutdown | ( | void |
|
) |
Shutdown storage plugin.
- Returns
- Error code indicating success or failure.
- Return values
-
BOOTLOADER_OKon success BOOTLOADER_ERROR_INIT_STORAGEon failure
| void storage_getInfo | ( | BootloaderStorageInformation_t * |
info
|
) |
Get information about the storage plugin running on the device.
- Parameters
-
[out] infoPointer to BootloaderStorageInformation_t struct
| int32_t storage_getSlotInfo | ( | uint32_t |
slotId,
|
| BootloaderStorageSlot_t * |
slot
|
||
| ) |
Get information about the layout of a storage slot
- Parameters
-
[in] slotIdSlot ID to get info about [out] slotPointer to BootloaderStorageSlot_t struct
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_getSlotMetadata | ( | BootloaderParserContext_t * |
context,
|
| ApplicationData_t * |
appInfo,
|
||
| uint32_t * |
bootloaderVersion
|
||
| ) |
Get information about the contents of a storage slot
- Note
- storage_initParseSlot must be called before calling this function to initialize the context.
- If the slot does not contain an application or a bootloader, the the corresponding values are set to zero.
- Parameters
-
[in] contextParsing context. Should be allocated by the application and initialized by calling storage_initParseSlot before calling this function. [out] appInfoPointer to ApplicationData_t struct [out] bootloaderVersionPointer to an unsigned integer representing the bootloader version number.
- Returns
- BOOTLOADER_OK on success
| int32_t storage_initParseSlot | ( | uint32_t |
slotId,
|
| BootloaderParserContext_t * |
context,
|
||
| size_t |
contextSize
|
||
| ) |
Initialize the context variable for checking a slot and trying to parse the image contained in it.
- Parameters
-
[in] slotIdSlot to check for valid image [in] contextPointer to BootloaderParserContext_t struct [in] contextSizeLength of the context struct
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_PARSE_BASE range
| int32_t storage_verifySlot | ( | BootloaderParserContext_t * |
context,
|
| BootloaderParserCallback_t |
metadataCallback
|
||
| ) |
Check the given slot for a valid image. Call this function continuously until it stops returning. BOOTLOADER_ERROR_PARSE_CONTINUE .
The function returns BOOTLOADER_ERROR_PARSE_SUCCESS if the image in the slot was successfully verified. For detailed information on the parsed image, see imageProperties in the context variable.
- Parameters
-
[in] contextPointer to BootloaderImageParsingContext_t struct [in] metadataCallbackFunctionpointer which will be called with any binary metadata that might be contained within the image.
- Returns
- BOOTLOADER_ERROR_PARSE_CONTINUE if the parsing is not complete, BOOTLOADER_ERROR_PARSE_SUCCESS on success.
| bool storage_upgradeSeFromSlot | ( | uint32_t |
slotId
|
) |
Upgrade SE using image contained in a slot.
- Note
- This function assumes the image located in the slotId has been verified first.
- Parameters
-
slotIdSlot ID to bootload from
- Returns
- True if the operation succeeded
| bool storage_bootloadBootloaderFromSlot | ( | uint32_t |
slotId,
|
| uint32_t |
version
|
||
| ) |
Bootload a bootloader image contained in a slot
- Note
- This function assumes the image located in the slotId has been verified first.
- Parameters
-
slotIdSlot ID to bootload from versionVersion number of new bootloader
- Returns
- True if operation succeeded
| bool storage_bootloadApplicationFromSlot | ( | uint32_t |
slotId,
|
| uint32_t |
version
|
||
| ) |
Bootload an image contained in a slot.
- Note
- This function assumes the image located in slotId has been verified first.
- Parameters
-
slotIdSlot ID to bootload from versionCached version number of the image contained in the slot (used for downgrade prevention)
- Returns
- True if the operation succeeded
| int32_t storage_eraseSlot | ( | uint32_t |
slotId
|
) |
Erase the contents of a storage slot including all data and metadata.
- Parameters
-
slotIdID of the slot.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_readSlot | ( | uint32_t |
slotId,
|
| uint32_t |
offset,
|
||
| uint8_t * |
buffer,
|
||
| size_t |
numBytes
|
||
| ) |
Read a number of words from a storage slot.
- Parameters
-
slotIdID of the slot. offsetThe offset into the slot in bytes. bufferPointer to buffer to store read data in. numBytesNumber of bytes to read.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_writeSlot | ( | uint32_t |
slotId,
|
| uint32_t |
offset,
|
||
| uint8_t * |
data,
|
||
| size_t |
numBytes
|
||
| ) |
Write a number of words to a storage slot.
- Parameters
-
slotIdID of the slot. offsetThe offset into the slot in bytes. dataPointer to data to write. numBytesLength of data to write. Must be a multiple of 4.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_readRaw | ( | uint32_t |
address,
|
| uint8_t * |
buffer,
|
||
| size_t |
numBytes
|
||
| ) |
Read number of words from raw storage.
- Parameters
-
addressThe raw address of the storage. bufferPointer to the buffer to store read data in. numBytesNumber of bytes to read.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_writeRaw | ( | uint32_t |
address,
|
| uint8_t * |
data,
|
||
| size_t |
numBytes
|
||
| ) |
Write a number of words to raw storage.
- Parameters
-
addressThe raw address of the storage. dataPointer to data to write. numBytesLength of data to write. Must be a multiple of 4.
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| int32_t storage_eraseRaw | ( | uint32_t |
address,
|
| size_t |
length
|
||
| ) |
Erase the raw storage.
- Parameters
-
addressStart address of the region to erase lengthNumber of bytes to erase
- Note
- Some devices, such as Flash-based storages, have restrictions on the alignment and size of erased regions. The details of the limitations of a particular storage can be found by reading the BootloaderStorageInformation_t struct using storage_getInfo .
- Returns
- BOOTLOADER_OK on success, else error code in BOOTLOADER_ERROR_STORAGE_BASE range
| bool storage_isBusy | ( | void |
|
) |
Poll the storage implementation and check whether it is busy.
- Returns
- True if the storage is busy