MainBootloaderTable_t Struct ReferenceApplication Interface > Common Application Interface
Description
Address table for the Main Bootloader.
Definition at line
114
of file
btl_interface.h
.
#include <
btl_interface.h
>
Data Fields |
|
| BootloaderHeader_t | header |
|
Header of the Main Bootloader table.
|
|
| uint32_t | size |
|
Size of the Main Bootloader.
|
|
| BareBootTable_t * | startOfAppSpace |
|
Start address of the application.
|
|
| uint32_t * | endOfAppSpace |
|
End address of the allocated application space.
|
|
| uint32_t | capabilities |
|
Capabilities of the bootloader.
|
|
| int32_t(* | init )(void) |
|
Initialize bootloader for use from application.
|
|
| int32_t(* | deinit )(void) |
|
Deinitialize bootloader after use from application.
|
|
| bool(* | verifyApplication )(uint32_t startAddress) |
|
Verify application.
|
|
| int32_t(* | initParser )( BootloaderParserContext_t *context, size_t contextSize) |
|
Initialize parser.
|
|
| int32_t(* | parseBuffer )( BootloaderParserContext_t *context, const BootloaderParserCallbacks_t *callbacks, uint8_t data[], size_t numBytes) |
|
Parse a buffer.
|
|
| const BootloaderStorageFunctions_t * | storage |
|
Function table for storage plugin.
|
|
The documentation for this struct was generated from the following file:
-
btl_interface.h