BootloaderParserCallbacks_t Struct ReferenceApplication Interface > Application Parser Interface

Description

Function pointers to parser callbacks.

Definition at line 57 of file btl_interface_parser.h.

#include <btl_interface_parser.h>

Data Fields

void * context
 Opaque pointer passed to the callback functions.
 
BootloaderParserCallback_t applicationCallback
 Callback function pointer for application image data.
 
BootloaderParserCallback_t metadataCallback
 Callback function pointer for image metadata.
 
BootloaderParserCallback_t bootloaderCallback
 Callback function pointer for bootloader upgrade image data.
 

The documentation for this struct was generated from the following file:
  • btl_interface_parser.h