FlashBootloader Core
Description
Interface to internal flash.
Used for writing application images to the main flash.
Functions |
|
| void | flash_init (void) |
| void | flash_deinit (void) |
| bool | flash_erasePage (uint32_t address) |
| bool | flash_writeWord (uint32_t address, uint32_t data) |
| bool | flash_writeBuffer (uint32_t address, void *data, size_t length) |
Function Documentation
| void flash_init | ( | void |
|
) |
Initialize the flash driver
| void flash_deinit | ( | void |
|
) |
Deinitialize the flash driver
| bool flash_erasePage | ( | uint32_t |
address
|
) |
Erase a flash page
- Parameters
-
[in] addressStart address of the flash page to erase.
- Returns
- True if operation was successful
| bool flash_writeWord | ( | uint32_t |
address,
|
| uint32_t |
data
|
||
| ) |
Write a word to internal flash
- Parameters
-
addressAddress in internal flash to write word to dataWord to write
- Returns
- True if operation was successful
| bool flash_writeBuffer | ( | uint32_t |
address,
|
| void * |
data,
|
||
| size_t |
length
|
||
| ) |
Write buffer to internal flash
- Parameters
-
addressStarting address to write data to. Must be half-word aligned. dataData buffer to write to internal flash lengthAmount of bytes in the data buffer to write
- Returns
- True if operation was successful