BootloaderStorageImplementationInformation_t Struct ReferenceApplication Interface > Application Storage Interface
Description
Information about the bootloader storage implementation.
Definition at line
57
of file
btl_interface_storage.h
.
#include <
btl_interface_storage.h
>
Data Fields |
|
| uint16_t | version |
|
The version of this data structure.
|
|
| uint16_t | capabilitiesMask |
|
A bitmask describing the capabilities of this particular storage.
|
|
| uint32_t | pageEraseMs |
|
Maximum time it takes to erase a page. (in milliseconds)
|
|
| uint32_t | partEraseMs |
|
Maximum time it takes to erase the entire part. (in milliseconds)
|
|
| uint32_t | pageSize |
|
The size of a single erasable page in bytes.
|
|
| uint32_t | partSize |
|
The total size of the storage in bytes.
|
|
| const char *const | partDescription |
|
Pointer to a string describing the attached storage.
|
|
| uint8_t | wordSizeBytes |
|
The number of bytes in a word for the storage.
|
|
The documentation for this struct was generated from the following file:
-
btl_interface_storage.h