Reset InformationApplication Interface > Common Application Interface
Description
Passing information when resetting into and out of the bootloader.
To signal the bootloader to run, the application needs to write the BootloaderResetCause_t structure to the first address of RAM, setting BootloaderResetCause_t::reason to BOOTLOADER_RESET_REASON_BOOTLOAD .
The reset cause is only valid if BootloaderResetCause_t::signature is set to BOOTLOADER_RESET_SIGNATURE_VALID .
When the bootloader reboots back into the app, it sets the reset reason to BOOTLOADER_RESET_REASON_GO if the bootload succeeded, or BOOTLOADER_RESET_REASON_BADIMAGE if the bootload failed due to errors when parsing the upgrade image.
- Note
- The reset information is automatically filled out before reset if the bootloader_rebootAndInstall function is called.
Data Structures |
|
| struct | BootloaderResetCause_t |
|
Reset cause of the bootloader.
|
|
Macros |
|
| #define | BOOTLOADER_RESET_REASON_UNKNOWN 0x0200u |
|
Unknown bootloader cause (should never occur)
|
|
| #define | BOOTLOADER_RESET_REASON_GO 0x0201u |
|
Bootloader caused reset telling app to run.
|
|
| #define | BOOTLOADER_RESET_REASON_BOOTLOAD 0x0202u |
|
Application requested that bootloader runs.
|
|
| #define | BOOTLOADER_RESET_REASON_BADIMAGE 0x0203u |
|
Bootloader detected bad external upgrade image.
|
|
| #define | BOOTLOADER_RESET_REASON_FATAL 0x0204u |
|
Fatal Error or assert in bootloader.
|
|
| #define | BOOTLOADER_RESET_REASON_FORCE 0x0205u |
|
Forced bootloader activation.
|
|
| #define | BOOTLOADER_RESET_REASON_OTAVALID 0x0206u |
|
OTA Bootloader mode activation.
|
|
| #define | BOOTLOADER_RESET_REASON_DEEPSLEEP 0x0207u |
|
Bootloader initiated deep sleep.
|
|
| #define | BOOTLOADER_RESET_REASON_BADAPP 0x0208u |
|
Application verification failed.
|
|
| #define | BOOTLOADER_RESET_REASON_UPGRADE 0x0209u |
|
Bootloader requested that first stage upgrades main bootloader.
|
|
| #define | BOOTLOADER_RESET_REASON_TIMEOUT 0x020Au |
|
Bootloader timed out waiting for upgrade image.
|
|
| #define | BOOTLOADER_RESET_SIGNATURE_VALID 0xF00Fu |
|
Reset signature is valid.
|
|
| #define | BOOTLOADER_RESET_SIGNATURE_INVALID 0xC33Cu |
|
Reset signature is invalid.
|
|