DEVINFO_TypeDef Struct ReferenceDevices > EFM32TG_DEVINFO

Definition at line 47 of file efm32tg_devinfo.h .

Data Fields

__IM uint32_t ADC0CAL0
__IM uint32_t ADC0CAL1
__IM uint32_t ADC0CAL2
__IM uint32_t AUXHFRCOCAL0
__IM uint32_t AUXHFRCOCAL1
__IM uint32_t CAL
__IM uint32_t DAC0CAL0
__IM uint32_t DAC0CAL1
__IM uint32_t DAC0CAL2
__IM uint32_t HFRCOCAL0
__IM uint32_t HFRCOCAL1
__IM uint32_t MEMINFO
__IM uint32_t MSIZE
__IM uint32_t PART
uint32_t RESERVED0 [2]
uint32_t RESERVED2 [2]
__IM uint32_t UNIQUEH
__IM uint32_t UNIQUEL

Field Documentation

__IM uint32_t DEVINFO_TypeDef::ADC0CAL0

ADC0 Calibration register 0

Definition at line 49 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL1

ADC0 Calibration register 1

Definition at line 50 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::ADC0CAL2

ADC0 Calibration register 2

Definition at line 51 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL0

AUXHFRCO calibration register 0

Definition at line 56 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::AUXHFRCOCAL1

AUXHFRCO calibration register 1

Definition at line 57 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::CAL

Calibration temperature and checksum

Definition at line 48 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DAC0CAL0

DAC calibrartion register 0

Definition at line 53 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DAC0CAL1

DAC calibrartion register 1

Definition at line 54 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::DAC0CAL2

DAC calibrartion register 2

Definition at line 55 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL0

HFRCO calibration register 0

Definition at line 58 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::HFRCOCAL1

HFRCO calibration register 1

Definition at line 59 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MEMINFO

Memory information

Definition at line 60 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::MSIZE

Flash and SRAM Memory size in KiloBytes

Definition at line 64 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::PART

Part description

Definition at line 65 of file efm32tg_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED0[2]

Reserved

Definition at line 52 of file efm32tg_devinfo.h .

uint32_t DEVINFO_TypeDef::RESERVED2[2]

Reserved

Definition at line 61 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEH

High 32 bits of device unique number

Definition at line 63 of file efm32tg_devinfo.h .

__IM uint32_t DEVINFO_TypeDef::UNIQUEL

Low 32 bits of device unique number

Definition at line 62 of file efm32tg_devinfo.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/ efm32tg_devinfo.h