USART_InitSync_TypeDef Struct ReferenceEMLIB > USART
Synchronous mode init structure.
Definition at line
457
of file
em_usart.h
.
#include <
em_usart.h
>
Data Fields |
|
bool | autoTx |
uint32_t | baudrate |
USART_ClockMode_TypeDef | clockMode |
USART_Databits_TypeDef | databits |
USART_Enable_TypeDef | enable |
bool | master |
bool | msbf |
USART_PrsRxCh_TypeDef | prsRxCh |
bool | prsRxEnable |
uint32_t | refFreq |
Field Documentation
bool USART_InitSync_TypeDef::autoTx |
Enable AUTOTX mode. Transmits as long as RX is not full. If TX is empty, underflows are generated.
Definition at line
491
of file
em_usart.h
.
Referenced by MIC_init() , and USART_InitSync() .
uint32_t USART_InitSync_TypeDef::baudrate |
Desired baudrate.
Definition at line
468
of file
em_usart.h
.
Referenced by MIC_init() , MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode |
Clock polarity/phase mode.
Definition at line
480
of file
em_usart.h
.
Referenced by SPIDRV_Init() , and USART_InitSync() .
USART_Databits_TypeDef USART_InitSync_TypeDef::databits |
Number of databits in frame.
Definition at line
471
of file
em_usart.h
.
Referenced by USART_InitSync() .
USART_Enable_TypeDef USART_InitSync_TypeDef::enable |
Specifies whether TX and/or RX shall be enabled when init completed.
Definition at line
459
of file
em_usart.h
.
Referenced by MIC_init() , USART_InitI2s() , and USART_InitSync() .
bool USART_InitSync_TypeDef::master |
Select if to operate in master or slave mode.
Definition at line
474
of file
em_usart.h
.
Referenced by SPIDRV_Init() , and USART_InitSync() .
bool USART_InitSync_TypeDef::msbf |
Select if to send most or least significant bit first.
Definition at line
477
of file
em_usart.h
.
Referenced by MICROSD_Init() , SPIDRV_Init() , and USART_InitSync() .
USART_PrsRxCh_TypeDef USART_InitSync_TypeDef::prsRxCh |
Select PRS channel for USART Rx. (Only valid if prsRxEnable is true).
Definition at line
487
of file
em_usart.h
.
Referenced by USART_InitSync() .
bool USART_InitSync_TypeDef::prsRxEnable |
Enable USART Rx via PRS.
Definition at line
484
of file
em_usart.h
.
Referenced by USART_InitSync() .
uint32_t USART_InitSync_TypeDef::refFreq |
USART/UART reference clock assumed when configuring baudrate setup. Set it to 0 if currently configurated reference clock shall be used.
Definition at line
465
of file
em_usart.h
.
Referenced by USART_InitSync() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_usart.h