SYSTEM_CalAddrVal_TypeDef Struct ReferenceEMLIB > SYSTEM

DEVINFO calibration address/value pair

Definition at line 275 of file em_system.h .

#include < em_system.h >

Data Fields

uint32_t address
uint32_t calValue

Field Documentation

uint32_t SYSTEM_CalAddrVal_TypeDef::address

Peripheral calibration register address

Definition at line 276 of file em_system.h .

Referenced by SYSTEM_GetCalibrationValue() .

uint32_t SYSTEM_CalAddrVal_TypeDef::calValue

Calibration value for register at address

Definition at line 277 of file em_system.h .

Referenced by SYSTEM_GetCalibrationValue() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_system.h