ADC_InitSingle_TypeDef Struct ReferenceEMLIB > ADC

Single conversion init structure.

Definition at line 962 of file em_adc.h .

#include < em_adc.h >

Data Fields

ADC_AcqTime_TypeDef acqTime
bool diff
bool fifoOverwrite
bool leftAdjust
ADC_NegSel_TypeDef negSel
ADC_PosSel_TypeDef posSel
bool prsEnable
ADC_PRSSEL_TypeDef prsSel
ADC_Ref_TypeDef reference
bool rep
ADC_Res_TypeDef resolution
bool singleDmaEm2Wu

Field Documentation

ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime

Acquisition time (in ADC clock cycles).

Definition at line 970 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .

bool ADC_InitSingle_TypeDef::diff

Select if single ended or differential input.

Definition at line 1001 of file em_adc.h .

Referenced by ADC_InitSingle() .

bool ADC_InitSingle_TypeDef::fifoOverwrite

When true, the FIFO overwrites old data when full. If false, then the FIFO discards new data. The SCANOF IRQ is triggered in both cases.

Definition at line 1020 of file em_adc.h .

Referenced by ADC_InitSingle() .

bool ADC_InitSingle_TypeDef::leftAdjust

Select if left adjustment should be done.

Definition at line 1007 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel

Select negative input for single channel conversion mode. Negative input is grounded for single ended (non-differential) converison.

Definition at line 997 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel

Select positive input for for single channel conversion mode.

Definition at line 991 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

bool ADC_InitSingle_TypeDef::prsEnable

Peripheral reflex system trigger enable.

Definition at line 1004 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel

Peripheral reflex system trigger selection. Only applicable if prsEnable is enabled.

Definition at line 967 of file em_adc.h .

Referenced by ADC_InitSingle() , and adcInit() .

ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference

Sample reference selection. Notice that for external references, the ADC calibration register must be set explicitly.

Definition at line 976 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::rep

Select if continuous conversion until explicit stop.

Definition at line 1010 of file em_adc.h .

Referenced by ADC_InitSingle() .

ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution

Sample resolution.

Definition at line 979 of file em_adc.h .

Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .

bool ADC_InitSingle_TypeDef::singleDmaEm2Wu

When true, DMA is available in EM2 for single conversion

Definition at line 1014 of file em_adc.h .

Referenced by ADC_InitSingle() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_adc.h