LESENSE_DecCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE decoder control descriptor structure.
Definition at line
671
of file
em_lesense.h
.
#include <
em_lesense.h
>
Data Fields |
|
| bool | chkState |
| LESENSE_DecInput_TypeDef | decInput |
| bool | hystIRQ |
| bool | hystPRS0 |
| bool | hystPRS1 |
| bool | hystPRS2 |
| uint32_t | initState |
| bool | intMap |
| LESENSE_PRSSel_TypeDef | prsChSel0 |
| LESENSE_PRSSel_TypeDef | prsChSel1 |
| LESENSE_PRSSel_TypeDef | prsChSel2 |
| LESENSE_PRSSel_TypeDef | prsChSel3 |
| bool | prsCount |
Field Documentation
| bool LESENSE_DecCtrlDesc_TypeDef::chkState |
Set to enable the decoder to check the present state in addition to the states defined in TCONF.
Definition at line
680
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput |
Select the input to the LESENSE decoder.
Definition at line
673
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ |
Set to enable hysteresis in the decoder for suppressing interrupt requests.
Definition at line
700
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 0.
Definition at line
688
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 1.
Definition at line
692
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2 |
Set to enable hysteresis in the decoder for suppressing changes on PRS channel 2.
Definition at line
696
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| uint32_t LESENSE_DecCtrlDesc_TypeDef::initState |
Initial state of the LESENSE decoder.
Definition at line
676
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::intMap |
When set, a transition from state x in the decoder will set interrupt flag CHx.
Definition at line
684
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0 |
Select PRS channel input for bit 0 of the LESENSE decoder.
Definition at line
707
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1 |
Select PRS channel input for bit 1 of the LESENSE decoder.
Definition at line
710
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2 |
Select PRS channel input for bit 2 of the LESENSE decoder.
Definition at line
713
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3 |
Select PRS channel input for bit 3 of the LESENSE decoder.
Definition at line
716
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_DecCtrlDesc_TypeDef::prsCount |
Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.
Definition at line
704
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h