LESENSE_CoreCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Core control (LESENSE_CTRL) descriptor structure.
Definition at line
490
of file
em_lesense.h
.
#include <
em_lesense.h
>
Field Documentation
| LESENSE_BiasMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::biasMode |
| bool LESENSE_CoreCtrlDesc_TypeDef::bufOverWr |
Set to true in order to always make LESENSE write to the result buffer, even if it is full.
Definition at line
515
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_BufTrigLevel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::bufTrigLevel |
Select trigger conditions for interrupt and DMA.
Definition at line
518
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::debugRun |
Set to true to keep LESENSE running in debug mode.
Definition at line
527
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::dualSample |
Set to true to sample both ACMPs simultaneously.
Definition at line
507
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP0 |
Set to true to invert ACMP0 output.
Definition at line
501
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::invACMP1 |
Set to true to invert ACMP1 output.
Definition at line
504
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_PRSSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::prsSel |
Select PRS source for scan start if scanMode is set to lesensePrsPulse.
Definition at line
495
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_ScanConfSel_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanConfSel |
Select scan configuration register usage strategy.
Definition at line
498
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_ScanMode_TypeDef LESENSE_CoreCtrlDesc_TypeDef::scanStart |
Select scan start mode to control how the scan start is being triggered.
Definition at line
492
of file
em_lesense.h
.
Referenced by CAPLESENSE_setupLESENSE() , and LESENSE_Init() .
| bool LESENSE_CoreCtrlDesc_TypeDef::storeScanRes |
Set to true in order to to store SCANRES in RAM (accessible via RESDATA) after each scan.
Definition at line
511
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
| LESENSE_DMAWakeUp_TypeDef LESENSE_CoreCtrlDesc_TypeDef::wakeupOnDMA |
Configure trigger condition for DMA wakeup from EM2.
Definition at line
521
of file
em_lesense.h
.
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h