LESENSE_ConfAltEx_TypeDef Struct ReferenceEMLIB > LESENSE
Configuration structure for alternate excitation.
Definition at line
945
of file
em_lesense.h
.
#include <
em_lesense.h
>
Data Fields |
|
| LESENSE_AltExDesc_TypeDef | AltEx [16] |
| LESENSE_AltExMap_TypeDef | altExMap |
Field Documentation
| LESENSE_AltExDesc_TypeDef LESENSE_ConfAltEx_TypeDef::AltEx[16] |
Alternate excitation channel descriptors. When altExMap==lesenseAltExMapALTEX only the 8 first descriptors are used. In this mode they describe the configuration of the LES_ALTEX0-7 pins. When altExMap==lesenseAltExMapACMP all 16 descriptors are used. In this mode they describe the configuration of the 16 possible ACMP0-1 excitation channels. Please refer to the user manual for a complete mapping of the routing. NOTE: Some parameters in the descriptors are not valid when altExMap==lesenseAltExMapACMP. Please refer to the definition of the LESENSE_AltExDesc_TypeDef structure for details regarding which parameters are valid.
Definition at line
961
of file
em_lesense.h
.
Referenced by LESENSE_AltExConfig() .
| LESENSE_AltExMap_TypeDef LESENSE_ConfAltEx_TypeDef::altExMap |
Select alternate excitation mapping.
Definition at line
947
of file
em_lesense.h
.
Referenced by LESENSE_AltExConfig() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h