CSEN_Init_TypeDef Struct ReferenceEMLIB > CSEN
CSEN init structure, common for all measurement modes.
Definition at line
341
of file
em_csen.h
.
#include <
em_csen.h
>
Data Fields |
|
| bool | cpAccuracyHi |
| CSEN_InputSel_TypeDef | input0To7 |
| CSEN_InputSel_TypeDef | input16To23 |
| CSEN_InputSel_TypeDef | input24To31 |
| CSEN_InputSel_TypeDef | input32To39 |
| CSEN_InputSel_TypeDef | input40To47 |
| CSEN_InputSel_TypeDef | input48To55 |
| CSEN_InputSel_TypeDef | input56To63 |
| CSEN_InputSel_TypeDef | input8To15 |
| bool | keepWarm |
| bool | localSense |
| CSEN_PCPrescale_TypeDef | pcPrescale |
| uint8_t | pcReload |
| CSEN_PRSSel_TypeDef | prsSel |
| uint8_t | warmUpCount |
Field Documentation
| bool CSEN_Init_TypeDef::cpAccuracyHi |
Requests system charge pump high accuracy mode.
Definition at line
343
of file
em_csen.h
.
Referenced by CSEN_Init() .
| CSEN_InputSel_TypeDef CSEN_Init_TypeDef::input0To7 |
CSEN input to APORT channel mapping.
Definition at line
364
of file
em_csen.h
.
Referenced by CSEN_Init() .
| bool CSEN_Init_TypeDef::keepWarm |
Keeps the converter warm allowing continuous conversions.
Definition at line
349
of file
em_csen.h
.
Referenced by CSEN_Init() .
| bool CSEN_Init_TypeDef::localSense |
Disables external kelvin connection and senses capacitor locally.
Definition at line
346
of file
em_csen.h
.
Referenced by CSEN_Init() .
| CSEN_PCPrescale_TypeDef CSEN_Init_TypeDef::pcPrescale |
| uint8_t CSEN_Init_TypeDef::pcReload |
| CSEN_PRSSel_TypeDef CSEN_Init_TypeDef::prsSel |
Peripheral reflex system trigger selection.
Definition at line
361
of file
em_csen.h
.
Referenced by CSEN_Init() .
| uint8_t CSEN_Init_TypeDef::warmUpCount |
Converter warmup time is warmUpCount + 3 converter clock cycles.
Definition at line
352
of file
em_csen.h
.
Referenced by CSEN_Init() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_csen.h