textdisplay.h File Reference
Text display interface.
- Version
- 5.4.0
License
Copyright 2015 Silicon Labs, Inc. http://www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file textdisplay.h
.
#include <stdbool.h>
#include "emstatus.h
"
Data Structures | |
struct | TEXTDISPLAY_Config_t |
Macros | |
#define | TEXTDISPLAY_EMSTATUS_ALREADY_INITIALIZED (TEXTDISPLAY_EMSTATUS_BASE | 3) |
#define | TEXTDISPLAY_EMSTATUS_INVALID_PARAM (TEXTDISPLAY_EMSTATUS_BASE | 1) |
#define | TEXTDISPLAY_EMSTATUS_NOT_ENOUGH_MEMORY (TEXTDISPLAY_EMSTATUS_BASE | 5) |
#define | TEXTDISPLAY_EMSTATUS_NOT_INITIALIZED (TEXTDISPLAY_EMSTATUS_BASE | 6) |
#define | TEXTDISPLAY_EMSTATUS_NOT_SUPPORTED (TEXTDISPLAY_EMSTATUS_BASE | 4) |
#define | TEXTDISPLAY_EMSTATUS_OK (0) |
#define | TEXTDISPLAY_EMSTATUS_OUT_OF_RANGE (TEXTDISPLAY_EMSTATUS_BASE | 2) |
Typedefs | |
typedef struct TEXTDISPLAY_Config_t | TEXTDISPLAY_Config_t |
typedef void * | TEXTDISPLAY_Handle_t |
Functions | |
EMSTATUS | TEXTDISPLAY_Delete (TEXTDISPLAY_Handle_t handle) |
Delete a text display device. | |
EMSTATUS | TEXTDISPLAY_LfToCrLf (TEXTDISPLAY_Handle_t handle, bool on) |
Enable or disable LF to CR+LF conversion. | |
EMSTATUS | TEXTDISPLAY_New (TEXTDISPLAY_Config_t *config, TEXTDISPLAY_Handle_t *handle) |
Create a new text display device. | |
EMSTATUS | TEXTDISPLAY_WriteChar (TEXTDISPLAY_Handle_t handle, char c) |
Write a single character to a text display. | |
EMSTATUS | TEXTDISPLAY_WriteString (TEXTDISPLAY_Handle_t handle, const char *str) |
Write a string of characters to a text display. | |