ACMP_TypeDef Struct ReferenceDevices > ACMP

ACMP Register Declaration

Definition at line 49 of file efr32fg12p_acmp.h .

#include < efr32fg12p_acmp.h >

Data Fields

__IM uint32_t APORTCONFLICT
__IM uint32_t APORTREQ
__IOM uint32_t CTRL
__IOM uint32_t EXTIFCTRL
__IOM uint32_t HYSTERESIS0
__IOM uint32_t HYSTERESIS1
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INPUTSEL
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [4]
__IOM uint32_t ROUTELOC0
__IOM uint32_t ROUTEPEN
__IM uint32_t STATUS

Field Documentation

__IM uint32_t ACMP_TypeDef::APORTCONFLICT

APORT Conflict Status Register

Definition at line 59 of file efr32fg12p_acmp.h .

__IM uint32_t ACMP_TypeDef::APORTREQ

APORT Request Status Register

Definition at line 58 of file efr32fg12p_acmp.h .

__IOM uint32_t ACMP_TypeDef::CTRL

Control Register

Definition at line 50 of file efr32fg12p_acmp.h .

Referenced by ACMP_CapsenseInit() , ACMP_Disable() , ACMP_Enable() , ACMP_GPIOSetup() , ACMP_Init() , and ACMP_Reset() .

__IOM uint32_t ACMP_TypeDef::EXTIFCTRL

External Override Interface Control

Definition at line 66 of file efr32fg12p_acmp.h .

Referenced by ACMP_ExternalInputSelect() .

__IOM uint32_t ACMP_TypeDef::HYSTERESIS0

Hysteresis 0 Register

Definition at line 60 of file efr32fg12p_acmp.h .

Referenced by ACMP_CapsenseInit() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .

__IOM uint32_t ACMP_TypeDef::HYSTERESIS1

Hysteresis 1 Register

Definition at line 61 of file efr32fg12p_acmp.h .

Referenced by ACMP_CapsenseInit() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .

__IOM uint32_t ACMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 56 of file efr32fg12p_acmp.h .

Referenced by ACMP_IntDisable() , ACMP_IntEnable() , ACMP_IntGetEnabled() , and ACMP_Reset() .

__IM uint32_t ACMP_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efr32fg12p_acmp.h .

Referenced by ACMP_IntGet() , and ACMP_IntGetEnabled() .

__IOM uint32_t ACMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efr32fg12p_acmp.h .

Referenced by ACMP_IntClear() , and ACMP_Reset() .

__IOM uint32_t ACMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efr32fg12p_acmp.h .

Referenced by ACMP_IntSet() .

__IOM uint32_t ACMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 51 of file efr32fg12p_acmp.h .

Referenced by ACMP_CapsenseChannelSet() , ACMP_CapsenseInit() , ACMP_ChannelSet() , ACMP_Init() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .

uint32_t ACMP_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 57 of file efr32fg12p_acmp.h .

uint32_t ACMP_TypeDef::RESERVED1[4]

Reserved for future use

Definition at line 63 of file efr32fg12p_acmp.h .

__IOM uint32_t ACMP_TypeDef::ROUTELOC0

I/O Routing Location Register

Definition at line 65 of file efr32fg12p_acmp.h .

Referenced by ACMP_GPIOSetup() .

__IOM uint32_t ACMP_TypeDef::ROUTEPEN

I/O Routing Pine Enable Register

Definition at line 64 of file efr32fg12p_acmp.h .

Referenced by ACMP_GPIOSetup() .

__IM uint32_t ACMP_TypeDef::STATUS

Status Register

Definition at line 52 of file efr32fg12p_acmp.h .

Referenced by ACMP_ExternalInputSelect() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/ efr32fg12p_acmp.h