LESENSE_PerCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE peripheral control descriptor structure.
Definition at line 568
of file em_lesense.h
.
#include <
em_lesense.h
>
Field Documentation
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode |
Configure how LESENSE controls ACMP 0.
Definition at line 608
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode |
Configure how LESENSE controls ACMP 1.
Definition at line 611
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data |
Configure DAC channel 0 data control.
Definition at line 570
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_PerCtrlDesc_TypeDef::dacCh0En |
When set to true, LESENSE controls DAC channel 0.
Definition at line 630
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data |
Configure DAC channel 1 data control.
Definition at line 583
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_PerCtrlDesc_TypeDef::dacCh1En |
When set to true, LESENSE controls DAC channel 1.
Definition at line 635
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_PerCtrlDesc_TypeDef::dacScan |
When set to true the DAC is only enabled once for each scan. When set to false the DAC is enabled before every channel measurement.
Definition at line 619
of file em_lesense.h
.
Referenced by LESENSE_Init().
bool LESENSE_PerCtrlDesc_TypeDef::dacStartupHalf |
When set to true the DAC is started a half clock cycle before sensor interaction starts. When set to false, a full clock cycle is used.
Definition at line 625
of file em_lesense.h
.
Referenced by LESENSE_Init().
LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode |
Configure how LESENSE controls ACMPs and the DAC in idle mode.
Definition at line 614
of file em_lesense.h
.
Referenced by LESENSE_Init().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_lesense.h