CRYOTIMER_Init_TypeDef Struct ReferenceEMLIB > CRYOTIMER
CRYOTIMER initialization structure.
Definition at line 179
of file em_cryotimer.h
.
#include <
em_cryotimer.h
>
Data Fields | |
bool | debugRun |
bool | em4Wakeup |
bool | enable |
CRYOTIMER_Osc_TypeDef | osc |
CRYOTIMER_Period_TypeDef | period |
CRYOTIMER_Presc_TypeDef | presc |
Field Documentation
bool CRYOTIMER_Init_TypeDef::debugRun |
Enable/disable timer counting during debug halt.
Definition at line 184
of file em_cryotimer.h
.
Referenced by CRYOTIMER_Init().
bool CRYOTIMER_Init_TypeDef::em4Wakeup |
Enable/disable EM4 Wakeup.
Definition at line 187
of file em_cryotimer.h
.
Referenced by CRYOTIMER_Init().
bool CRYOTIMER_Init_TypeDef::enable |
Enable/disable counting when initialization is completed.
Definition at line 181
of file em_cryotimer.h
.
Referenced by CRYOTIMER_Init().
CRYOTIMER_Osc_TypeDef CRYOTIMER_Init_TypeDef::osc |
Select the oscillator for the CRYOTIMER.
Definition at line 190
of file em_cryotimer.h
.
Referenced by CRYOTIMER_Init().
CRYOTIMER_Period_TypeDef CRYOTIMER_Init_TypeDef::period |
Period between wakeup event/interrupt.
Definition at line 196
of file em_cryotimer.h
.
Referenced by CRYOTIMER_Init().
CRYOTIMER_Presc_TypeDef CRYOTIMER_Init_TypeDef::presc |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_cryotimer.h