TRNG_TypeDef Struct ReferenceDevices > TRNG

TRNG Register Declaration

Definition at line 49 of file efr32fg12p_trng.h .

#include < efr32fg12p_trng.h >

Data Fields

__IOM uint32_t CONTROL
__IM uint32_t FIFO
__IM uint32_t FIFODEPTH
__IM uint32_t FIFOLEVEL
__IOM uint32_t INITWAITVAL
__IOM uint32_t KEY0
__IOM uint32_t KEY1
__IOM uint32_t KEY2
__IOM uint32_t KEY3
uint32_t RESERVED0 [1]
uint32_t RESERVED1 [3]
uint32_t RESERVED2 [50]
__IOM uint32_t STATUS
__IOM uint32_t TESTDATA

Field Documentation

__IOM uint32_t TRNG_TypeDef::CONTROL

Main Control Register

Definition at line 50 of file efr32fg12p_trng.h .

__IM uint32_t TRNG_TypeDef::FIFO

FIFO Data

Definition at line 64 of file efr32fg12p_trng.h .

__IM uint32_t TRNG_TypeDef::FIFODEPTH

FIFO Depth Register

Definition at line 53 of file efr32fg12p_trng.h .

__IM uint32_t TRNG_TypeDef::FIFOLEVEL

FIFO Level Register

Definition at line 51 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::INITWAITVAL

Initial Wait Counter

Definition at line 62 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::KEY0

Key Register 0

Definition at line 54 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::KEY1

Key Register 1

Definition at line 55 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::KEY2

Key Register 2

Definition at line 56 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::KEY3

Key Register 3

Definition at line 57 of file efr32fg12p_trng.h .

uint32_t TRNG_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 52 of file efr32fg12p_trng.h .

uint32_t TRNG_TypeDef::RESERVED1[3]

Reserved for future use

Definition at line 60 of file efr32fg12p_trng.h .

uint32_t TRNG_TypeDef::RESERVED2[50]

Reserved for future use

Definition at line 63 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::STATUS

Status Register

Definition at line 61 of file efr32fg12p_trng.h .

__IOM uint32_t TRNG_TypeDef::TESTDATA

Test Data Register

Definition at line 58 of file efr32fg12p_trng.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/ efr32fg12p_trng.h