DMA_DESCRIPTOR_TypeDef Struct ReferenceDevices > DMA Descriptor
DMA_DESCRIPTOR Register Declaration
Definition at line 48
of file efr32fg12p_dma_descriptor.h
.
#include <
efr32fg12p_dma_descriptor.h
>
Data Fields | |
__IOM uint32_t | CTRL |
__IOM void *__IOM | DST |
__IOM void *__IOM | LINK |
__IOM void *__IOM | SRC |
Field Documentation
__IOM uint32_t DMA_DESCRIPTOR_TypeDef::CTRL |
DMA control register
Definition at line 51
of file efr32fg12p_dma_descriptor.h
.
__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::DST |
DMA destination address
Definition at line 53
of file efr32fg12p_dma_descriptor.h
.
__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::LINK |
DMA link address
Definition at line 54
of file efr32fg12p_dma_descriptor.h
.
__IOM void* __IOM DMA_DESCRIPTOR_TypeDef::SRC |
DMA source address
Definition at line 52
of file efr32fg12p_dma_descriptor.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32FG12P/Include/
efr32fg12p_dma_descriptor.h