emstatus.h File Reference

EMSTATUS definitions.

Version
5.5.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file emstatus.h .

#include <stdint.h>
#include "em_types.h"

Macros

#define DISPLAY_EMSTATUS_BASE (0x8011UL << 16)
#define EMSTATUS_OK (0)
#define PAL_EMSTATUS_BASE (0x8013UL << 16)
#define TEXTDISPLAY_EMSTATUS_BASE (0x8012UL << 16)

Macro Definition Documentation

#define DISPLAY_EMSTATUS_BASE   (0x8011UL << 16)

EMSTATUS base codes for display modules. EMSTATUS base code of DISPLAY driver interface.

Definition at line 26 of file emstatus.h .

#define EMSTATUS_OK   (0)

Common EMSTATUS codes: Operation successful.

Definition at line 23 of file emstatus.h .

#define PAL_EMSTATUS_BASE   (0x8013UL << 16)

EMSTATUS base code of PAL interface.

Definition at line 28 of file emstatus.h .

#define TEXTDISPLAY_EMSTATUS_BASE   (0x8012UL << 16)

EMSTATUS base code of TEXTDISPLAY module.

Definition at line 27 of file emstatus.h .