tftamapped.c File Reference

EFM32GG_DK3750, TFT Initialization and setup for Adress Mapped mode.

Version
5.5.0

License

Copyright 2015 Silicon Labs, Inc. http://www.silabs.com

This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.

Definition in file tftamapped.c .

#include <stdbool.h>
#include " em_device.h "
#include " em_gpio.h "
#include " em_ebi.h "
#include " bsp.h "
#include " tftamapped.h "
#include "dmd/ssd2119/dmd_ssd2119.h"
#include " glib/glib.h "

Functions

bool TFT_AddressMappedInit (void)
TFT initialize or reinitialize to Address Mapped Mode Assumes EBI has been configured correctly in BSP_Init(BSP_INIT_DK_EBI)

Variables

static bool runOnce = true

Variable Documentation

bool runOnce = true
static

Flag to indicate that we need to initialize once if starting up in

Definition at line 27 of file tftamapped.c .

Referenced by TFT_AddressMappedInit() .