ACMP_TypeDef Struct ReferenceDevices > EFM32TG_ACMP

Definition at line 48 of file efm32tg_acmp.h.

Data Fields

__IOM uint32_t CTRL
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t IFS
 
__IOM uint32_t INPUTSEL
 
__IOM uint32_t ROUTE
 
__IM uint32_t STATUS
 

Field Documentation

__IOM uint32_t ACMP_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32tg_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Disable(), ACMP_Enable(), ACMP_GPIOSetup(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efm32tg_acmp.h.

Referenced by ACMP_IntDisable(), ACMP_IntEnable(), ACMP_IntGetEnabled(), and ACMP_Reset().

__IM uint32_t ACMP_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32tg_acmp.h.

Referenced by ACMP_IntGet(), and ACMP_IntGetEnabled().

__IOM uint32_t ACMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32tg_acmp.h.

Referenced by ACMP_IntClear(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32tg_acmp.h.

Referenced by ACMP_IntSet().

__IOM uint32_t ACMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 50 of file efm32tg_acmp.h.

Referenced by ACMP_CapsenseChannelSet(), ACMP_CapsenseInit(), ACMP_ChannelSet(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::ROUTE

I/O Routing Register

Definition at line 56 of file efm32tg_acmp.h.

Referenced by ACMP_GPIOSetup().

__IM uint32_t ACMP_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32tg_acmp.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/efm32tg_acmp.h