CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU
LFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.
Definition at line 1401
of file em_cmu.h
.
#include <
em_cmu.h
>
Data Fields | |
CMU_LFXOBoost_TypeDef | boost |
CMU_OscMode_TypeDef | mode |
uint8_t | timeout |
Field Documentation
CMU_LFXOBoost_TypeDef CMU_LFXOInit_TypeDef::boost |
CMU_OscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
uint8_t CMU_LFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_cmu.h